Utility Functions#
Utility functions for applications on SoC.
Functions#
sl_status_t
sl_btmesh_pop_event(sl_btmesh_msg_t *event)
bool
sl_btmesh_event_pending(void)
uint32_t
Function Documentation#
sl_btmesh_pop_event#
sl_status_t sl_btmesh_pop_event (sl_btmesh_msg_t * event)
Parameters
N/A | event | the pointer for storing the new event |
Get the next event that requires processing by user application. Application is not blocked if no event is waiting.
Returns
SL_STATUS_OK if a new event is returned, or SL_STATUS_NOT_FOUND if no event is waiting; other value indicates an error occurred
Definition at line
22984
of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_event_pending#
bool sl_btmesh_event_pending (void )
Parameters
N/A |
Check whether events are in queue pending for processing. Call sl_btmesh_pop_event to process pending events.
Returns
true if event is pending; false otherwise
Definition at line
22992
of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_event_pending_len#
uint32_t sl_btmesh_event_pending_len (void )
Parameters
N/A |
Check whether events are in queue pending for processing and return the next event length in bytes if events are pending. Call sl_btmesh_pop_event to process pending events.
Returns
the next event length if event is pending; 0 otherwise
Definition at line
23001
of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h