Data structure of the relay event.

Public Attributes#

int8_t
uint8_t

Public Attribute Documentation#

destination_address#

uint16_t sl_btmesh_evt_diagnostic_relay_s::destination_address

Message destination address


Definition at line 22442 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

source_address#

uint16_t sl_btmesh_evt_diagnostic_relay_s::source_address

Message source address


Definition at line 22443 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

rssi#

int8_t sl_btmesh_evt_diagnostic_relay_s::rssi

RSSI value of the relayed message. Units: dBm.


Definition at line 22444 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

ttl#

uint8_t sl_btmesh_evt_diagnostic_relay_s::ttl

Time-to-Live value of the relayed or proxied message


Definition at line 22446 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h