Data structure of the distribution_status event.

Public Attributes#

uint16_t
uint8_t
uint8_t
uint16_t
uint16_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_fw_dist_client_distribution_status_s::elem_index

Client model element index


Definition at line 18506 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

server_address#

uint16_t sl_btmesh_evt_fw_dist_client_distribution_status_s::server_address

Unicast address of the server


Definition at line 18507 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

status#

uint8_t sl_btmesh_evt_fw_dist_client_distribution_status_s::status

Enum sl_btmesh_fw_dist_server_dist_status_t. Status code returned


Definition at line 18508 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

phase#

uint8_t sl_btmesh_evt_fw_dist_client_distribution_status_s::phase

Enum sl_btmesh_fw_dist_client_dist_phase_t. Phase of the Distribution Server


Definition at line 18511 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

group_address#

uint16_t sl_btmesh_evt_fw_dist_client_distribution_status_s::group_address

Distribution group address. Ignore if no distribution is active.


Definition at line 18514 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

appkey_index#

uint16_t sl_btmesh_evt_fw_dist_client_distribution_status_s::appkey_index

Distribution app key index. Ignore if no distribution is active.


Definition at line 18516 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

distributor_ttl#

uint8_t sl_btmesh_evt_fw_dist_client_distribution_status_s::distributor_ttl

TTL used by the Distributor. Ignore if no distribution is active.


Definition at line 18518 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

timeout_base#

uint16_t sl_btmesh_evt_fw_dist_client_distribution_status_s::timeout_base

Timeout Base value used in BLOB Transfer


Definition at line 18520 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

transfer_mode#

uint8_t sl_btmesh_evt_fw_dist_client_distribution_status_s::transfer_mode

Transfer Mode used in BLOB Transfer


Definition at line 18521 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

apply_immediately#

uint8_t sl_btmesh_evt_fw_dist_client_distribution_status_s::apply_immediately

1 if the Update Policy is Verify and Apply, otherwise 0. Ignore if no distribution is active.


Definition at line 18522 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

fw_list_index#

uint16_t sl_btmesh_evt_fw_dist_client_distribution_status_s::fw_list_index

Index of the firmware in the Distributor's Firmware List


Definition at line 18525 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h