Data structure of the fw_status event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_fw_dist_client_fw_status_s::elem_index
Client model element index
Definition at line
18582
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server_address#
uint16_t sl_btmesh_evt_fw_dist_client_fw_status_s::server_address
Unicast address of the server
Definition at line
18583
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
status#
uint8_t sl_btmesh_evt_fw_dist_client_fw_status_s::status
Enum sl_btmesh_fw_dist_server_dist_status_t. Status code returned
Definition at line
18584
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
num_entries#
uint16_t sl_btmesh_evt_fw_dist_client_fw_status_s::num_entries
Number of images stored on the Distributor
Definition at line
18587
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
index#
uint16_t sl_btmesh_evt_fw_dist_client_fw_status_s::index
Index of the queried firmware on the server. 0xffff if not found.
Definition at line
18588
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
fwid#
uint8array sl_btmesh_evt_fw_dist_client_fw_status_s::fwid
FWID of the firmware that was queried. Empty if get_by_index was used and no such index exists.
Definition at line
18590
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h