Data structure of the receivers_list_end event.

Public Attributes#

uint16_t
uint16_t
uint16_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_end_s::elem_index

Client model element index


Definition at line 18442 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

server_address#

uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_end_s::server_address

Unicast address of the server


Definition at line 18443 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

start_index#

uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_end_s::start_index

Starting index


Definition at line 18444 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

num_reported#

uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_end_s::num_reported

Number of entries reported


Definition at line 18445 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

nodes_list_size#

uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_end_s::nodes_list_size

Number of entries currently in the node list


Definition at line 18446 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h