Data structure of the receivers_status event.

Public Attributes#

uint16_t
uint8_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_fw_dist_client_receivers_status_s::elem_index

Client model element index


Definition at line 18381 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

server_address#

uint16_t sl_btmesh_evt_fw_dist_client_receivers_status_s::server_address

Unicast address of the server


Definition at line 18382 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

status#

uint8_t sl_btmesh_evt_fw_dist_client_receivers_status_s::status

Enum sl_btmesh_fw_dist_server_dist_status_t. Status code returned


Definition at line 18383 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

nodes_list_size#

uint16_t sl_btmesh_evt_fw_dist_client_receivers_status_s::nodes_list_size

Number of entries currently in the node list


Definition at line 18386 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h