sl_btmesh_evt_fw_dist_server_upload_oob_start_req#
Upload OOB Start request.
The preceding event sl_btmesh_evt_fw_dist_server_upload_oob_start_uri contains the URI to use in combination with the FWID of this event. The application should execute the Check Firmware OOB procedure and then respond to this event with the command sl_btmesh_fw_dist_server_upload_oob_start_rsp according to the information received OOB.
Modules#
sl_btmesh_evt_fw_dist_server_upload_oob_start_req_s
Typedefs#
Macros#
#define
Identifier of the upload_oob_start_req event.
Typedef Documentation#
sl_btmesh_evt_fw_dist_server_upload_oob_start_req_t#
typedef struct sl_btmesh_evt_fw_dist_server_upload_oob_start_req_s sl_btmesh_evt_fw_dist_server_upload_oob_start_req_t
Definition at line
17726
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
Macro Definition Documentation#
sl_btmesh_evt_fw_dist_server_upload_oob_start_req_id#
#define sl_btmesh_evt_fw_dist_server_upload_oob_start_req_idValue:
0x115800a8
Identifier of the upload_oob_start_req event.
Definition at line
17713
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h