Data structure of the info_status_update_uri event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_fw_update_client_info_status_update_uri_s::elem_index
Client model element index
Definition at line
13189
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server_address#
uint16_t sl_btmesh_evt_fw_update_client_info_status_update_uri_s::server_address
Unicast address of the server
Definition at line
13190
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
index#
uint8_t sl_btmesh_evt_fw_update_client_info_status_update_uri_s::index
Index of this URI in the Firmware Information List
Definition at line
13191
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
count#
uint8_t sl_btmesh_evt_fw_update_client_info_status_update_uri_s::count
Total number of entries in the Firmware Information List
Definition at line
13193
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
update_uri#
uint8array sl_btmesh_evt_fw_update_client_info_status_update_uri_s::update_uri
Update URI
Definition at line
13195
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h