sl_btmesh_evt_fw_update_server_distributor_self_update_req#
This event can only be generated if both Distribution Server and Update Server functionality are used on the same node.
This event signals that the Initiator has added this node to the list of nodes to be updated; that is, the node is asked to update itself using an image already present in the Distribution Server's Firmware List. The command sl_btmesh_fw_update_server_distributor_self_update_rsp must be called to accept or reject the self-update request.
Modules#
sl_btmesh_evt_fw_update_server_distributor_self_update_req_s
Typedefs#
Macros#
#define
Identifier of the distributor_self_update_req event.
Typedef Documentation#
sl_btmesh_evt_fw_update_server_distributor_self_update_req_t#
typedef struct sl_btmesh_evt_fw_update_server_distributor_self_update_req_s sl_btmesh_evt_fw_update_server_distributor_self_update_req_t
Definition at line
16035
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
Macro Definition Documentation#
sl_btmesh_evt_fw_update_server_distributor_self_update_req_id#
#define sl_btmesh_evt_fw_update_server_distributor_self_update_req_idValue:
0x075700a8
Identifier of the distributor_self_update_req event.
Definition at line
16013
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h