sl_btmesh_evt_generic_server_state_changed#

Cached model state changed.

This may happen either as a direct result of model state update by the application, in which case the event can be ignored, or because the update of one model state resulted in an update of a bound model state according to the Mesh model specification. In this case, the application should update its own value accordingly.

Modules#

sl_btmesh_evt_generic_server_state_changed_s

Macros#

#define

Identifier of the state_changed event.

Typedef Documentation#

sl_btmesh_evt_generic_server_state_changed_t#

typedef struct sl_btmesh_evt_generic_server_state_changed_s sl_btmesh_evt_generic_server_state_changed_t

Definition at line 5917 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_evt_generic_server_state_changed_id#

#define sl_btmesh_evt_generic_server_state_changed_id
Value:
0x011f00a8

Identifier of the state_changed event.


Definition at line 5897 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h