sl_btmesh_evt_health_client_server_status#
Receiving a Health Server fault status message generates this event.
The Client model may receive a status message because:
it made a sl_btmesh_health_client_get to which a Server model responded
it made a sl_btmesh_health_client_clear to which a Server model responded
it made a sl_btmesh_health_client_test to which a Server model responded
Modules#
sl_btmesh_evt_health_client_server_status_s
Typedefs#
Macros#
#define
sl_btmesh_evt_health_client_server_status_id 0x001a00a8
Identifier of the server_status event.
Typedef Documentation#
sl_btmesh_evt_health_client_server_status_t#
typedef struct sl_btmesh_evt_health_client_server_status_s sl_btmesh_evt_health_client_server_status_t
Definition at line
4627
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
Macro Definition Documentation#
sl_btmesh_evt_health_client_server_status_id#
#define sl_btmesh_evt_health_client_server_status_idValue:
0x001a00a8
Identifier of the server_status event.
Definition at line
4602
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h