Data structure of the mode_status event.

Public Attributes#

uint16_t
uint16_t

Public Attribute Documentation#

destination_address#

uint16_t sl_btmesh_evt_lc_client_mode_status_s::destination_address

Address of the client or the group address to which it was published.


Definition at line 13564 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elem_index#

uint16_t sl_btmesh_evt_lc_client_mode_status_s::elem_index

Index of the element for which received the status.


Definition at line 13566 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

server_address#

uint16_t sl_btmesh_evt_lc_client_mode_status_s::server_address

Device which sent the status.


Definition at line 13568 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

appkey_index#

uint16_t sl_btmesh_evt_lc_client_mode_status_s::appkey_index

Appkey used by server_address.


Definition at line 13569 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

mode_status_value#

uint8_t sl_btmesh_evt_lc_client_mode_status_s::mode_status_value

Value reported by server.


Definition at line 13570 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h