Data structure of the property_status event.
Public Attribute Documentation#
destination_address#
uint16_t sl_btmesh_evt_lc_client_property_status_s::destination_address
Address of the client or the group address to which it was published.
Definition at line
13654
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elem_index#
uint16_t sl_btmesh_evt_lc_client_property_status_s::elem_index
Index of the element for which received the status.
Definition at line
13656
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server_address#
uint16_t sl_btmesh_evt_lc_client_property_status_s::server_address
Device which sent the status.
Definition at line
13658
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
appkey_index#
uint16_t sl_btmesh_evt_lc_client_property_status_s::appkey_index
Appkey used by server_address.
Definition at line
13659
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
property_id#
uint16_t sl_btmesh_evt_lc_client_property_status_s::property_id
Property ID
Definition at line
13660
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
property_value#
uint8array sl_btmesh_evt_lc_client_property_status_s::property_value
Property value
Definition at line
13661
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h