Data structure of the ambient_lux_level_updated event.

Public Attributes#

uint16_t
uint16_t

Public Attribute Documentation#

destination_address#

uint16_t sl_btmesh_evt_lc_server_ambient_lux_level_updated_s::destination_address

Message destination address


Definition at line 14169 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elem_index#

uint16_t sl_btmesh_evt_lc_server_ambient_lux_level_updated_s::elem_index

Index of the element where the update happened


Definition at line 14170 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

source_address#

uint16_t sl_btmesh_evt_lc_server_ambient_lux_level_updated_s::source_address

Message source address


Definition at line 14172 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

appkey_index#

uint16_t sl_btmesh_evt_lc_server_ambient_lux_level_updated_s::appkey_index

Message appkey index


Definition at line 14173 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

ambient_lux_level_value#

uint32_t sl_btmesh_evt_lc_server_ambient_lux_level_updated_s::ambient_lux_level_value

The updated value of the LC Ambient LuxLevel state


Definition at line 14174 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h