Data structure of the occupancy_updated event.

Public Attributes#

uint16_t
uint16_t

Public Attribute Documentation#

destination_address#

uint16_t sl_btmesh_evt_lc_server_occupancy_updated_s::destination_address

Message destination address if triggered by a message, 0 otherwise.


Definition at line 14138 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elem_index#

uint16_t sl_btmesh_evt_lc_server_occupancy_updated_s::elem_index

Index of the element where the update happened


Definition at line 14140 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

source_address#

uint16_t sl_btmesh_evt_lc_server_occupancy_updated_s::source_address

Message source address if triggered by a message, 0 otherwise.


Definition at line 14142 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

appkey_index#

uint16_t sl_btmesh_evt_lc_server_occupancy_updated_s::appkey_index

Message appkey index if triggered by a message, 0xFFFF otherwise.


Definition at line 14144 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

occupancy_value#

uint8_t sl_btmesh_evt_lc_server_occupancy_updated_s::occupancy_value

The updated value of the LC Occupancy state


Definition at line 14146 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h