Data structure of the fw_added event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_ncp_fw_list_fw_added_s::elem_index
Server model element index
Definition at line
20252
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
size#
uint32_t sl_btmesh_evt_ncp_fw_list_fw_added_s::size
Size of the image
Definition at line
20253
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
blob_id#
sl_bt_uuid_64_t sl_btmesh_evt_ncp_fw_list_fw_added_s::blob_id
BLOB ID that will be used to transmit the image
Definition at line
20254
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
fwid#
uint8array sl_btmesh_evt_ncp_fw_list_fw_added_s::fwid
Firmware ID of the image
Definition at line
20256
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h