Data structure of the private_gatt_proxy_status event.
Public Attribute Documentation#
result#
uint16_t sl_btmesh_evt_on_demand_private_proxy_client_private_gatt_proxy_status_s::result
SL_STATUS_OK if successful. Error code otherwise.
Definition at line
21948
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
handle#
uint32_t sl_btmesh_evt_on_demand_private_proxy_client_private_gatt_proxy_status_s::handle
Request handle
Definition at line
21949
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
value#
uint8_t sl_btmesh_evt_on_demand_private_proxy_client_private_gatt_proxy_status_s::value
On-Demand Private GATT proxy value of the node. Valid values are:
0: Advertising with Private Network Identity type cannot be enabled on demand
1-255: Advertising interval for Private Network Identity in seconds
Definition at line
21950
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h