Data structure of the scan_status event.
Public Attribute Documentation#
result#
uint16_t sl_btmesh_evt_remote_provisioning_client_scan_status_s::result
SL_STATUS_OK if successful. Error code otherwise.
Definition at line
19268
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server#
uint16_t sl_btmesh_evt_remote_provisioning_client_scan_status_s::server
Server address.
Definition at line
19269
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
status#
uint8_t sl_btmesh_evt_remote_provisioning_client_scan_status_s::status
Enum sl_btmesh_remote_provisioning_server_status_t. server status.
Definition at line
19270
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
state#
uint8_t sl_btmesh_evt_remote_provisioning_client_scan_status_s::state
Enum sl_btmesh_remote_provisioning_server_scan_state_t. Scan state.
Definition at line
19273
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
max_reports#
uint8_t sl_btmesh_evt_remote_provisioning_client_scan_status_s::max_reports
Maximum number of scanned items to be reported.
Definition at line
19276
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
timeout_sec#
uint8_t sl_btmesh_evt_remote_provisioning_client_scan_status_s::timeout_sec
Maximum available time for time left until the end of the Remote Provisioning Scan procedure.
Definition at line
19277
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h