Data structure of the action_status event.

Public Attributes#

uint16_t
uint16_t
uint8_t
uint8_t
uint16_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint16_t

Public Attribute Documentation#

client_address#

uint16_t sl_btmesh_evt_scheduler_client_action_status_s::client_address

Destination client model address


Definition at line 15139 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elem_index#

uint16_t sl_btmesh_evt_scheduler_client_action_status_s::elem_index

Client model element index


Definition at line 15140 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

server_address#

uint16_t sl_btmesh_evt_scheduler_client_action_status_s::server_address

Source server model address


Definition at line 15141 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

appkey_index#

uint16_t sl_btmesh_evt_scheduler_client_action_status_s::appkey_index

The application key index to use.


Definition at line 15142 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

index#

uint8_t sl_btmesh_evt_scheduler_client_action_status_s::index

Index of the Scheduler Register


Definition at line 15143 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

year#

uint8_t sl_btmesh_evt_scheduler_client_action_status_s::year

Scheduled year for the action


Definition at line 15144 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

month#

uint16_t sl_btmesh_evt_scheduler_client_action_status_s::month

Scheduled month for the action


Definition at line 15145 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

day#

uint8_t sl_btmesh_evt_scheduler_client_action_status_s::day

Scheduled day of the month for the action


Definition at line 15146 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

hour#

uint8_t sl_btmesh_evt_scheduler_client_action_status_s::hour

Scheduled hour for the action


Definition at line 15147 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

minute#

uint8_t sl_btmesh_evt_scheduler_client_action_status_s::minute

Scheduled minute for the action


Definition at line 15148 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

second#

uint8_t sl_btmesh_evt_scheduler_client_action_status_s::second

Scheduled second for the action


Definition at line 15149 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

day_of_week#

uint8_t sl_btmesh_evt_scheduler_client_action_status_s::day_of_week

Scheduled days of the week for the action


Definition at line 15150 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

action#

uint8_t sl_btmesh_evt_scheduler_client_action_status_s::action

Action to be performed at the scheduled time


Definition at line 15151 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

transition_time_ms#

uint32_t sl_btmesh_evt_scheduler_client_action_status_s::transition_time_ms

Transition time for this action


Definition at line 15152 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

scene_number#

uint16_t sl_btmesh_evt_scheduler_client_action_status_s::scene_number

Scene number to be used for some actions


Definition at line 15153 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h