Data structure of the series_status event.

Public Attributes#

uint16_t
uint16_t
uint8_t
uint16_t

Public Attribute Documentation#

client_address#

uint16_t sl_btmesh_evt_sensor_client_series_status_s::client_address

Destination client model address


Definition at line 12674 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elem_index#

uint16_t sl_btmesh_evt_sensor_client_series_status_s::elem_index

Client model element index


Definition at line 12675 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

server_address#

uint16_t sl_btmesh_evt_sensor_client_series_status_s::server_address

Source server model address


Definition at line 12676 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

appkey_index#

uint16_t sl_btmesh_evt_sensor_client_series_status_s::appkey_index

The application key index to use


Definition at line 12677 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

flags#

uint8_t sl_btmesh_evt_sensor_client_series_status_s::flags

No flags defined currently


Definition at line 12678 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

property_id#

uint16_t sl_btmesh_evt_sensor_client_series_status_s::property_id

Property ID for the sensor. Range: 0x0001 - 0x0ffff for a specific device property, the value 0x0000 is prohibited.


Definition at line 12679 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sensor_data#

uint8array sl_btmesh_evt_sensor_client_series_status_s::sensor_data

Byte array containing the serialized sequence of Sensor Serier Column states in the following format:

  • 1st Sensor Raw Value X, variable length raw value representing the left corner of a column

  • 1st Sensor Column Width, variable length raw value representing the width of the column

  • 1st Sensor Raw Value Y, variable length raw value representing the height of the column

  • ...

  • Nth Sensor Raw Value X, variable length raw value representing the left corner of a column

  • Nth Sensor Column Width, variable length raw value representing the width of the column

  • Nth Sensor Raw Value Y, variable length raw value representing the height of the column

If a Property ID or column requested does not exist at the server element, the reply Series Status message contains only the given Property ID.


Definition at line 12682 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h