Data structure of the setting_status event.

Public Attributes#

uint16_t
uint16_t
uint8_t
uint16_t
uint16_t

Public Attribute Documentation#

client_address#

uint16_t sl_btmesh_evt_sensor_client_setting_status_s::client_address

Destination client model address


Definition at line 12551 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elem_index#

uint16_t sl_btmesh_evt_sensor_client_setting_status_s::elem_index

Client model element index


Definition at line 12552 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

server_address#

uint16_t sl_btmesh_evt_sensor_client_setting_status_s::server_address

Source server model address


Definition at line 12553 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

appkey_index#

uint16_t sl_btmesh_evt_sensor_client_setting_status_s::appkey_index

The application key index to use


Definition at line 12554 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

flags#

uint8_t sl_btmesh_evt_sensor_client_setting_status_s::flags

No flags defined currently


Definition at line 12555 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

property_id#

uint16_t sl_btmesh_evt_sensor_client_setting_status_s::property_id

Property ID for the sensor. Range: 0x0001 - 0x0ffff for a specific device property, the value 0x0000 is prohibited.


Definition at line 12556 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

setting_id#

uint16_t sl_btmesh_evt_sensor_client_setting_status_s::setting_id

Sensor Setting Property ID field identifying the device property of a setting. Range: 0x0001 - 0xffff, 0x0000 is prohibited.


Definition at line 12559 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

raw_value#

uint8array sl_btmesh_evt_sensor_client_setting_status_s::raw_value

Sensor Setting raw value. Size and representation depends on the type defined by the Sensor Setting Property ID.


Definition at line 12562 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h