Data structure of the status event.
Public Attribute Documentation#
client_address#
uint16_t sl_btmesh_evt_sensor_client_status_s::client_address
Destination client model address
server_address#
uint16_t sl_btmesh_evt_sensor_client_status_s::server_address
Source server model address
appkey_index#
uint16_t sl_btmesh_evt_sensor_client_status_s::appkey_index
The application key index to use
sensor_data#
uint8array sl_btmesh_evt_sensor_client_status_s::sensor_data
Serialized Sensor Data consisting of one or more Sensor state for each sensor within the element. To simplify processing, the byte array is in TLV format:
- 1st Property ID: 16 bits 
- Value Length: 8 bits 
- Value: variable 
- 2nd Property ID: 16 bits 
- Value Length: 8 bits 
- Value: variable 
- ... 
If the requested Property ID does not exist at the server element, the reply contains only the given Property ID and zero length.