Data structure of the get_series_request event.

Public Attributes#

uint16_t
uint16_t
uint8_t
uint16_t

Public Attribute Documentation#

server_address#

uint16_t sl_btmesh_evt_sensor_server_get_series_request_s::server_address

Destination server address


Definition at line 11796 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elem_index#

uint16_t sl_btmesh_evt_sensor_server_get_series_request_s::elem_index

Server model element index


Definition at line 11797 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

client_address#

uint16_t sl_btmesh_evt_sensor_server_get_series_request_s::client_address

Source client address


Definition at line 11798 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

appkey_index#

uint16_t sl_btmesh_evt_sensor_server_get_series_request_s::appkey_index

The application key index to use


Definition at line 11799 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

flags#

uint8_t sl_btmesh_evt_sensor_server_get_series_request_s::flags

No flags defined currently


Definition at line 11800 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

property_id#

uint16_t sl_btmesh_evt_sensor_server_get_series_request_s::property_id

Property ID for the sensor. Range: 0x0001 - 0x0ffff for a specific device property, the value 0x0000 is prohibited.


Definition at line 11801 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

column_ids#

uint8array sl_btmesh_evt_sensor_server_get_series_request_s::column_ids

Optional raw values identifying starting and ending columns


Definition at line 11804 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h