Data structure of the get_settings_request event.
Public Attribute Documentation#
server_address#
uint16_t sl_btmesh_evt_sensor_setup_server_get_settings_request_s::server_address
Address the request was directed to, either the server's unicast address or a group address the server subscribes to
Definition at line
12088
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elem_index#
uint16_t sl_btmesh_evt_sensor_setup_server_get_settings_request_s::elem_index
Setup Server model element index
Definition at line
12091
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
client_address#
uint16_t sl_btmesh_evt_sensor_setup_server_get_settings_request_s::client_address
Requesting client model's address
Definition at line
12092
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
appkey_index#
uint16_t sl_btmesh_evt_sensor_setup_server_get_settings_request_s::appkey_index
The application key index to use
Definition at line
12093
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
flags#
uint8_t sl_btmesh_evt_sensor_setup_server_get_settings_request_s::flags
No flags defined currently
Definition at line
12094
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
property_id#
uint16_t sl_btmesh_evt_sensor_setup_server_get_settings_request_s::property_id
Property ID for the sensor. Range: 0x0001 - 0x0ffff for a specific device property, the value 0x0000 is prohibited.
Definition at line
12095
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h