sl_btmesh_evt_silabs_config_client_tx_status#

Node specific TX configuration state.

Received as a response to the sl_btmesh_silabs_config_client_set_tx and sl_btmesh_silabs_config_client_get_tx command.

Modules#

sl_btmesh_evt_silabs_config_client_tx_status_s

Macros#

#define

Identifier of the tx_status event.

Typedef Documentation#

sl_btmesh_evt_silabs_config_client_tx_status_t#

typedef struct sl_btmesh_evt_silabs_config_client_tx_status_s sl_btmesh_evt_silabs_config_client_tx_status_t

Definition at line 3902 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_evt_silabs_config_client_tx_status_id#

#define sl_btmesh_evt_silabs_config_client_tx_status_id
Value:
0x010100a8

Identifier of the tx_status event.


Definition at line 3883 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h