Data structure of the items_status event.
Public Attribute Documentation#
src#
uint16_t sl_btmesh_evt_solicitation_config_client_items_status_s::src
Server address
Definition at line
22069
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
dst#
uint16_t sl_btmesh_evt_solicitation_config_client_items_status_s::dst
Client address
Definition at line
22070
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
appkey_index#
uint16_t sl_btmesh_evt_solicitation_config_client_items_status_s::appkey_index
App key index
Definition at line
22071
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
range_start#
uint16_t sl_btmesh_evt_solicitation_config_client_items_status_s::range_start
15 least significant bits of the starting unicast address
Definition at line
22072
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
length_present#
uint8_t sl_btmesh_evt_solicitation_config_client_items_status_s::length_present
Indicates the presence or absence of the RangeLength field
Definition at line
22074
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
range_length#
uint8_t sl_btmesh_evt_solicitation_config_client_items_status_s::range_length
If present, containsNumber of addresses in the range (0x02 – 0xFF), otherwise 0
Definition at line
22076
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h