Data structure of the tai_utc_delta_status event.
Public Attribute Documentation#
client_address#
uint16_t sl_btmesh_evt_time_client_tai_utc_delta_status_s::client_address
Client address
Definition at line
16704
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elem_index#
uint16_t sl_btmesh_evt_time_client_tai_utc_delta_status_s::elem_index
Client model element index
Definition at line
16705
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server_address#
uint16_t sl_btmesh_evt_time_client_tai_utc_delta_status_s::server_address
Unicast address of the server
Definition at line
16706
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
appkey_index#
uint16_t sl_btmesh_evt_time_client_tai_utc_delta_status_s::appkey_index
App key index.
Definition at line
16707
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
tai_utc_delta_current#
int32_t sl_btmesh_evt_time_client_tai_utc_delta_status_s::tai_utc_delta_current
Current difference between TAI and UTC. Range is -255 to 32512.
Definition at line
16708
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
tai_utc_delta_new#
int32_t sl_btmesh_evt_time_client_tai_utc_delta_status_s::tai_utc_delta_new
Upcoming difference between TAI and UTC in seconds. Range is -255 to 32512.
Definition at line
16710
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
tai_of_delta_change#
uint64_t sl_btmesh_evt_time_client_tai_utc_delta_status_s::tai_of_delta_change
TAI seconds time of the upcoming TAI-UTC delta change
Definition at line
16712
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h