Data structure of the time_role_status event.

Public Attributes#

uint16_t
uint16_t
uint8_t

Public Attribute Documentation#

client_address#

uint16_t sl_btmesh_evt_time_client_time_role_status_s::client_address

Client address


Definition at line 16736 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elem_index#

uint16_t sl_btmesh_evt_time_client_time_role_status_s::elem_index

Client model element index


Definition at line 16737 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

server_address#

uint16_t sl_btmesh_evt_time_client_time_role_status_s::server_address

Unicast address of the server


Definition at line 16738 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

appkey_index#

uint16_t sl_btmesh_evt_time_client_time_role_status_s::appkey_index

App key index.


Definition at line 16739 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

time_role#

uint8_t sl_btmesh_evt_time_client_time_role_status_s::time_role

The Time Role for the element


Definition at line 16740 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h