Data structure of the time_status event.

Public Attributes#

uint16_t
uint16_t
uint64_t
uint8_t

Public Attribute Documentation#

client_address#

uint16_t sl_btmesh_evt_time_client_time_status_s::client_address

Client address


Definition at line 16636 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elem_index#

uint16_t sl_btmesh_evt_time_client_time_status_s::elem_index

Client model element index


Definition at line 16637 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

server_address#

uint16_t sl_btmesh_evt_time_client_time_status_s::server_address

Unicast address of the server


Definition at line 16638 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

appkey_index#

uint16_t sl_btmesh_evt_time_client_time_status_s::appkey_index

App key index.


Definition at line 16639 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

tai_seconds#

uint64_t sl_btmesh_evt_time_client_time_status_s::tai_seconds

The current TAI time in seconds


Definition at line 16640 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

subsecond#

uint8_t sl_btmesh_evt_time_client_time_status_s::subsecond

The sub-second time in units of 1/256th second


Definition at line 16641 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

uncertainty#

uint8_t sl_btmesh_evt_time_client_time_status_s::uncertainty

The estimated uncertainty in 10-millisecond steps


Definition at line 16642 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

time_authority#

uint8_t sl_btmesh_evt_time_client_time_status_s::time_authority

0 = No Time Authority, 1 = Time Authority


Definition at line 16644 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

tai_utc_delta#

int32_t sl_btmesh_evt_time_client_time_status_s::tai_utc_delta

Current difference between TAI and UTC in seconds. Range is -255 to 32512.


Definition at line 16645 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

time_zone_offset#

int16_t sl_btmesh_evt_time_client_time_status_s::time_zone_offset

The local time zone offset in 15-minute increments. Range is -64 to 191, representing -16 to 47.75 hours.


Definition at line 16647 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h