Key derivation#
API for key derivation and key agreement (ECDH, EC J-PAKE, HKDF, PBKDF2).
Contains key derivation functions (HKDF, PBKDF2) and key agreement functions (ECDH, ECJPAKE).
Modules#
Enumerations#
Roles in the EC J-PAKE exchange.
Typedefs#
Typedef sl_se_pbkdf2_prf_type_t to sl_se_hash_type_t in order to maintain backward compatibility.
Functions#
This function computes the shared secret with Elliptic Curve Diffie Hellman (ECDH) algorithm.
Check if an EC J-PAKE context is ready for use.
Derive the shared secret (TLS: Pre-Master Secret).
This clears an EC J-PAKE context and frees any embedded data structure.
Initialize an EC J-PAKE context.
Read and process the first round message (TLS: contents of the Client/ServerHello extension, excluding extension type and length bytes).
Read and process the second round message (TLS: contents of the Client/ServerKeyExchange).
Set up an EC J-PAKE context for use.
Generate and write the first round message (TLS: contents of the Client/ServerHello extension, excluding extension type and length bytes).
Generate and write the second round message (TLS: contents of the Client/ServerKeyExchange).
Derive a pseudorandom key from the input key material using HKDF.
Derive a pseudorandom key from the input key material using PBKDF2.
Macros#
Defines mapping the PBKDF2 PRFs to corresponding sl_se_hash_type_t values.
HMAC-SHA-1.
HMAC-SHA-224.
HMAC-SHA-256.
HMAC-SHA-384.
HMAC-SHA-512.
Enumeration Documentation#
sl_se_ecjpake_role_t#
sl_se_ecjpake_role_t
Roles in the EC J-PAKE exchange.
Enumerator | |
---|---|
SL_SE_ECJPAKE_CLIENT | Client. |
SL_SE_ECJPAKE_SERVER | Server. |
442
of file platform/security/sl_component/se_manager/inc/sl_se_manager_types.h
Typedef Documentation#
sl_se_pbkdf2_prf_type_t#
typedef sl_se_hash_type_t sl_se_pbkdf2_prf_type_t
Typedef sl_se_pbkdf2_prf_type_t to sl_se_hash_type_t in order to maintain backward compatibility.
Defines for mapping the PRF identifiers to the underlying hash enum values exists in sl_se_manager_defines.h.
478
of file platform/security/sl_component/se_manager/inc/sl_se_manager_types.h
Function Documentation#
sl_se_ecdh_compute_shared_secret
sl_status_t sl_se_ecdh_compute_shared_secret (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key_in_priv, const sl_se_key_descriptor_t *key_in_pub, const sl_se_key_descriptor_t *key_out)
This function computes the shared secret with Elliptic Curve Diffie Hellman (ECDH) algorithm.
[in] | cmd_ctx | Pointer to an SE command context object. |
[in] | key_in_priv | Our private key. |
[in] | key_in_pub | Their public key. |
[out] | key_out | Shared secret key. Montgomery curve result is one single coordinate. Other curve types result in one pair of coordinate. |
Performs Elliptic Curve Diffie Hellman shared secret computation.
Note
P-521 Elliptic Curve based Elliptic Curve Diffie Hellman (ECDH) expects a 544 bits (68 bytes) buffer for storing private keys, and a 1088 bits (136 bytes) buffer for storing public keys and shared secret. The first 23 bits of d, Qx, Qy and shared secret are padding bits to comply word-aligned addressing. The padding bits are ignored in the computation.
This function does not implement the value-checking of the shared secret as described in RFC7748 when using Montgomery keys.
In case of using custom domain curves, key_in_priv
defines the domain parameters. Moreover, key_in_pub
should always contain a public key. If key_in_pub contains a private key, sl_se_export_public_key() can be used to export the public key.
Returns
SL_STATUS_INVALID_KEY if
key_in_pub
does not contain a public key when using custom domain curves, otherwise an appropriate error code (sl_status.h).
112
of file platform/security/sl_component/se_manager/inc/sl_se_manager_key_derivation.h
sl_se_ecjpake_check#
sl_status_t sl_se_ecjpake_check (const sl_se_ecjpake_context_t *ctx)
Check if an EC J-PAKE context is ready for use.
[in] | ctx | The EC J-PAKE context to check. This must be initialized. |
Returns
SL_STATUS_OK when the command was executed successfully, otherwise an appropriate error code (sl_status.h).
131
of file platform/security/sl_component/se_manager/inc/sl_se_manager_key_derivation.h
sl_se_ecjpake_derive_secret#
sl_status_t sl_se_ecjpake_derive_secret (sl_se_ecjpake_context_t *ctx, unsigned char *buf, size_t len, size_t *olen)
Derive the shared secret (TLS: Pre-Master Secret).
[in] | ctx | The EC J-PAKE context to use. This must be initialized, set up and have performed both round one and two. |
[out] | buf | The buffer to write the derived secret to. This must be a writable buffer of length |
[in] | len | The length of |
[out] | olen | The address at which to store the total number of bytes written to |
Returns
SL_STATUS_OK when the command was executed successfully, otherwise an appropriate error code (sl_status.h).
156
of file platform/security/sl_component/se_manager/inc/sl_se_manager_key_derivation.h
sl_se_ecjpake_free#
sl_status_t sl_se_ecjpake_free (sl_se_ecjpake_context_t *ctx)
This clears an EC J-PAKE context and frees any embedded data structure.
[in] | ctx | The EC J-PAKE context to free. This may be |
Returns
SL_STATUS_OK when the command was executed successfully, otherwise an appropriate error code (sl_status.h).
174
of file platform/security/sl_component/se_manager/inc/sl_se_manager_key_derivation.h
sl_se_ecjpake_init#
sl_status_t sl_se_ecjpake_init (sl_se_ecjpake_context_t *ctx, sl_se_command_context_t *cmd_ctx)
Initialize an EC J-PAKE context.
[in] | ctx | The EC J-PAKE context to initialize. This must not be |
[in] | cmd_ctx | Pointer to an SE command context object. |
Returns
SL_STATUS_OK when the command was executed successfully, otherwise an appropriate error code (sl_status.h).
190
of file platform/security/sl_component/se_manager/inc/sl_se_manager_key_derivation.h
sl_se_ecjpake_read_round_one#
sl_status_t sl_se_ecjpake_read_round_one (sl_se_ecjpake_context_t *ctx, const unsigned char *buf, size_t len)
Read and process the first round message (TLS: contents of the Client/ServerHello extension, excluding extension type and length bytes).
[in] | ctx | The EC J-PAKE context to use. This must be initialized and set up. |
[in] | buf | The buffer holding the first round message. This must be a readable buffer of length |
[in] | len | The length in bytes of |
Returns
SL_STATUS_OK when the command was executed successfully, otherwise an appropriate error code (sl_status.h).
212
of file platform/security/sl_component/se_manager/inc/sl_se_manager_key_derivation.h
sl_se_ecjpake_read_round_two#
sl_status_t sl_se_ecjpake_read_round_two (sl_se_ecjpake_context_t *ctx, const unsigned char *buf, size_t len)
Read and process the second round message (TLS: contents of the Client/ServerKeyExchange).
[in] | ctx | The EC J-PAKE context to use. This must be initialized and set up and already have performed round one. |
[in] | buf | The buffer holding the second round message. This must be a readable buffer of length |
[in] | len | The length in bytes of |
Returns
SL_STATUS_OK when the command was executed successfully, otherwise an appropriate error code (sl_status.h).
236
of file platform/security/sl_component/se_manager/inc/sl_se_manager_key_derivation.h
sl_se_ecjpake_setup#
sl_status_t sl_se_ecjpake_setup (sl_se_ecjpake_context_t *ctx, sl_se_ecjpake_role_t role, sl_se_hash_type_t hash, uint32_t curve, const unsigned char *secret, size_t len)
Set up an EC J-PAKE context for use.
[in] | ctx | The EC J-PAKE context to set up. This must be initialized. |
[in] | role | The role of the caller. This must be either SL_SE_ECJPAKE_CLIENT or SL_SE_ECJPAKE_SERVER. |
[in] | hash | The identifier of the hash function to use, for example SL_SE_HASH_SHA256. |
[in] | curve | The identifier of the elliptic curve to use, for example SL_SE_KEY_TYPE_ECC_P256. |
[in] | secret | The pre-shared secret (passphrase). This must be a readable buffer of length |
[in] | len | The length of the pre-shared secret |
Note
Currently the only values for hash/curve allowed by the standard are SL_SE_HASH_SHA256 / SL_SE_KEY_TYPE_ECC_P256.
Returns
SL_STATUS_OK when the command was executed successfully, otherwise an appropriate error code (sl_status.h).
274
of file platform/security/sl_component/se_manager/inc/sl_se_manager_key_derivation.h
sl_se_ecjpake_write_round_one#
sl_status_t sl_se_ecjpake_write_round_one (sl_se_ecjpake_context_t *ctx, unsigned char *buf, size_t len, size_t *olen)
Generate and write the first round message (TLS: contents of the Client/ServerHello extension, excluding extension type and length bytes).
[in] | ctx | The EC J-PAKE context to use. This must be initialized and set up. |
[out] | buf | The buffer to write the contents to. This must be a writable buffer of length |
[in] | len | The length of |
[out] | olen | The address at which to store the total number of bytes written to |
Returns
SL_STATUS_OK when the command was executed successfully, otherwise an appropriate error code (sl_status.h).
304
of file platform/security/sl_component/se_manager/inc/sl_se_manager_key_derivation.h
sl_se_ecjpake_write_round_two#
sl_status_t sl_se_ecjpake_write_round_two (sl_se_ecjpake_context_t *ctx, unsigned char *buf, size_t len, size_t *olen)
Generate and write the second round message (TLS: contents of the Client/ServerKeyExchange).
[in] | ctx | The EC J-PAKE context to use. This must be initialized, set up, and already have performed round one. |
[out] | buf | The buffer to write the round two contents to. This must be a writable buffer of length |
[in] | len | The size of |
[out] | olen | The address at which to store the total number of bytes written to |
Returns
SL_STATUS_OK when the command was executed successfully, otherwise an appropriate error code (sl_status.h).
333
of file platform/security/sl_component/se_manager/inc/sl_se_manager_key_derivation.h
sl_se_derive_key_hkdf#
sl_status_t sl_se_derive_key_hkdf (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *in_key, sl_se_hash_type_t hash, const unsigned char *salt, size_t salt_len, const unsigned char *info, size_t info_len, sl_se_key_descriptor_t *out_key)
Derive a pseudorandom key from the input key material using HKDF.
[in] | cmd_ctx | Pointer to an SE command context object. |
[in] | in_key | Pointer to the input key material. |
[in] | hash | Which hashing algorithm to use. |
[in] | salt | An optional salt value (a non-secret random value). |
[in] | salt_len | The length of the salt. |
[in] | info | An optional context and application specific information string. |
[in] | info_len | The length of info. |
[inout] | out_key | Pointer to the generated key material. The length member of out_key is used to request a given length of the generated key. |
Returns
SL_STATUS_OK if the signature is successfully verified, otherwise an appropriate error code (sl_status.h).
375
of file platform/security/sl_component/se_manager/inc/sl_se_manager_key_derivation.h
sl_se_derive_key_pbkdf2#
sl_status_t sl_se_derive_key_pbkdf2 (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *in_key, sl_se_pbkdf2_prf_type_t prf, const unsigned char *salt, size_t salt_len, uint32_t iterations, sl_se_key_descriptor_t *out_key)
Derive a pseudorandom key from the input key material using PBKDF2.
[in] | cmd_ctx | Pointer to an SE command context object. |
[in] | in_key | Pointer to the input key material. |
[in] | prf | The underlying psuedorandom function (PRF) to use in the algorithm. The most common choice of HMAC-SHA-{1, 224, 256, 384, 512} is supported on all Series-2 devices (with Vault High Security). Newer chips, EFR32xG23 and later, also support usage of AES-CMAC-PRF-128. |
[in] | salt | An optional salt value (a non-secret random value). |
[in] | salt_len | The length of the salt. |
[in] | iterations | The number of iterations to use. Up to 16384 iterations is supported. |
[inout] | out_key | Pointer to the generated key material. The length member of out_key is used to request a given length of the generated key. |
Returns
SL_STATUS_OK if the signature is successfully verified, otherwise an appropriate error code (sl_status.h).
417
of file platform/security/sl_component/se_manager/inc/sl_se_manager_key_derivation.h
Macro Definition Documentation#
SL_SE_PRF_AES_CMAC_128#
#define SL_SE_PRF_AES_CMAC_128Value:
SL_SE_HASH_NONE
Defines mapping the PBKDF2 PRFs to corresponding sl_se_hash_type_t values.
CMAC-AES-128
241
of file platform/security/sl_component/se_manager/inc/sl_se_manager_defines.h
SL_SE_PRF_HMAC_SHA1#
#define SL_SE_PRF_HMAC_SHA1Value:
SL_SE_HASH_SHA1
HMAC-SHA-1.
242
of file platform/security/sl_component/se_manager/inc/sl_se_manager_defines.h
SL_SE_PRF_HMAC_SHA224#
#define SL_SE_PRF_HMAC_SHA224Value:
SL_SE_HASH_SHA224
HMAC-SHA-224.
243
of file platform/security/sl_component/se_manager/inc/sl_se_manager_defines.h
SL_SE_PRF_HMAC_SHA256#
#define SL_SE_PRF_HMAC_SHA256Value:
SL_SE_HASH_SHA256
HMAC-SHA-256.
244
of file platform/security/sl_component/se_manager/inc/sl_se_manager_defines.h
SL_SE_PRF_HMAC_SHA384#
#define SL_SE_PRF_HMAC_SHA384Value:
SL_SE_HASH_SHA384
HMAC-SHA-384.
245
of file platform/security/sl_component/se_manager/inc/sl_se_manager_defines.h
SL_SE_PRF_HMAC_SHA512#
#define SL_SE_PRF_HMAC_SHA512Value:
SL_SE_HASH_SHA512
HMAC-SHA-512.
246
of file platform/security/sl_component/se_manager/inc/sl_se_manager_defines.h