Signature#
Digital Signature Algorithms (ECDSA, EdDSA).
API for using digital signatures with the SE.
Functions#
This function computes Elliptic-Curve Cryptography (ECC) digital signatures of a message.
This function verifies Elliptic-Curve Cryptography (ECC) digital signatures of a message.
Function Documentation#
sl_se_ecc_sign#
sl_status_t sl_se_ecc_sign (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key, sl_se_hash_type_t hash_alg, bool hashed_message, const unsigned char *message, size_t message_len, unsigned char *signature, size_t signature_len)
This function computes Elliptic-Curve Cryptography (ECC) digital signatures of a message.
[in] | cmd_ctx | Pointer to an SE command context object. |
[in] | key | Pointer to sl_se_key_descriptor_t structure. |
[in] | hash_alg | Which hashing algorithm to use. Ignored for EdDSA keys, since EdDSA always uses SHA-512 for Ed25519 and SHA-3 for Ed448. |
[in] | hashed_message | The input message is a message digest. Ignored for EdDSA keys, and treated as false. |
[in] | message | The message to be used to compute the signature. |
[in] | message_len | The length of message. |
[out] | signature | The computed signature. |
[in] | signature_len | The length of the computed signature. |
Note
Edwards-curve Digital Signature Algorithm (EdDSA) generates a message digest using the input message for computing signatures. The input parameters
hash_alg
andhashed_message
do not apply for EdDSA.
P-521 Elliptic Curve for Elliptic Curve Digital Signature Algorithm (ECDSA) expects a 544 bits (68 bytes) buffer for storing private keys, and a 1088 bits (136 bytes) buffer for storing public keys and signatures. The first 23 bits of d, Qx, Qy, R and S are padding bits to comply word-aligned addressing.
Returns
SL_STATUS_OK when the command was executed successfully, otherwise an appropiate error code (sl_status.h).
113
of file platform/security/sl_component/se_manager/inc/sl_se_manager_signature.h
sl_se_ecc_verify#
sl_status_t sl_se_ecc_verify (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key, sl_se_hash_type_t hash_alg, bool hashed_message, const unsigned char *message, size_t message_len, const unsigned char *signature, size_t signature_len)
This function verifies Elliptic-Curve Cryptography (ECC) digital signatures of a message.
[in] | cmd_ctx | Pointer to an SE command context object. |
[in] | key | Pointer to sl_se_key_descriptor_t structure. |
[in] | hash_alg | Which hashing algorithm to use. Ignored for EdDSA keys, since EdDSA always uses SHA-512 for Ed25519 and SHA-3 for Ed448. |
[in] | hashed_message | The input message is a message digest. Ignored for EdDSA keys, and treated as false. |
[in] | message | The message to be used to compute signatures. |
[in] | message_len | The length of message. |
[in] | signature | The signature to be verified. |
[in] | signature_len | The length of signature. |
Note
The input parameters
hash_alg
andhashed_message
do not apply for Edwards-curve Digital Signature Algorithm (EdDSA).
P-521 Elliptic Curve for Elliptic Curve Digital Signature Algorithm (ECDSA) expects a 544 bits (68 bytes) buffer for storing private keys, and a 1088 bits (136 bytes) buffer for storing public keys and signatures. The first 23 bits of d, Qx, Qy, R and S are padding bits to comply word-aligned addressing.
Returns
SL_STATUS_OK if the signature is successfully verified, otherwise an appropiate error code (sl_status.h).
167
of file platform/security/sl_component/se_manager/inc/sl_se_manager_signature.h