Each attribute has it's metadata stored in such struct.
There is only one of these per attribute across all endpoints.
Public Attributes#
uint8_t
Public Attribute Documentation#
attributeId#
EmberAfAttributeId EmberAfAttributeMetadata::attributeId
Attribute ID, according to ZCL specs.
Definition at line
154
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h
attributeType#
EmberAfAttributeType EmberAfAttributeMetadata::attributeType
Attribute type, according to ZCL specs.
Definition at line
158
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h
size#
uint8_t EmberAfAttributeMetadata::size
Size of this attribute in bytes.
Definition at line
162
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h
mask#
EmberAfAttributeMask EmberAfAttributeMetadata::mask
Attribute mask, tagging attribute with specific functionality. See ATTRIBUTE_MASK_ macros defined in att-storage.h.
Definition at line
168
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h
defaultValue#
EmberAfDefaultOrMinMaxAttributeValue EmberAfAttributeMetadata::defaultValue
Pointer to the default value union. Actual value stored depends on the mask.
Definition at line
173
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h