Zigbee Internet Client/Server Remote Binding struct.

Public Attributes#

EmberEUI64
uint16_t
EmberEUI64
EmberEUI64

Public Attribute Documentation#

targetEUI64#

EmberEUI64 EmberAfRemoteBindingStruct::targetEUI64

Definition at line 1813 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h

sourceEndpoint#

uint8_t EmberAfRemoteBindingStruct::sourceEndpoint

Definition at line 1814 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h

destEndpoint#

uint8_t EmberAfRemoteBindingStruct::destEndpoint

Definition at line 1815 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h

clusterId#

uint16_t EmberAfRemoteBindingStruct::clusterId

Definition at line 1816 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h

destEUI64#

EmberEUI64 EmberAfRemoteBindingStruct::destEUI64

Definition at line 1817 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h

sourceEUI64#

EmberEUI64 EmberAfRemoteBindingStruct::sourceEUI64

Definition at line 1818 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h