Public Attribute Documentation#

valid#

bool EmberAfPluginMessagingClientMessage::valid

Definition at line 959 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h

active#

bool EmberAfPluginMessagingClientMessage::active

Definition at line 960 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h

esiBitmask#

EmberAfPluginEsiManagementBitmask EmberAfPluginMessagingClientMessage::esiBitmask

Definition at line 961 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h

clientEndpoint#

uint8_t EmberAfPluginMessagingClientMessage::clientEndpoint

Definition at line 962 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h

messageId#

uint32_t EmberAfPluginMessagingClientMessage::messageId

Definition at line 963 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h

messageControl#

uint8_t EmberAfPluginMessagingClientMessage::messageControl

Definition at line 964 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h

startTime#

uint32_t EmberAfPluginMessagingClientMessage::startTime

Definition at line 965 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h

endTime#

uint32_t EmberAfPluginMessagingClientMessage::endTime

Definition at line 966 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h

durationInMinutes#

uint16_t EmberAfPluginMessagingClientMessage::durationInMinutes

Definition at line 967 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h

message#

uint8_t EmberAfPluginMessagingClientMessage::message[EMBER_AF_PLUGIN_MESSAGING_CLIENT_MESSAGE_SIZE+1]

Definition at line 968 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h