Public Attributes#

uint32_t
uint8_t
uint32_t

Public Attribute Documentation#

providerId#

uint32_t EmberAfDeviceManagementTenancy::providerId

Definition at line 1671 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h

issuerEventId#

uint32_t EmberAfDeviceManagementTenancy::issuerEventId

Definition at line 1672 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h

tariffType#

uint8_t EmberAfDeviceManagementTenancy::tariffType

Definition at line 1673 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h

implementationDateTime#

uint32_t EmberAfDeviceManagementTenancy::implementationDateTime

Definition at line 1676 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h

tenancy#

uint32_t EmberAfDeviceManagementTenancy::tenancy

Definition at line 1677 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h