The EmberAFClusterCommand is a struct wrapper for all the data pertaining to a command which comes in over the air. This enables struct is used to encapsulate a command in a single place on the stack and pass a pointer to that location around during command processing.
Public Attribute Documentation#
apsFrame#
EmberApsFrame* EmberAfClusterCommand::apsFrame
APS frame for the incoming message
Definition at line
414
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h
type#
EmberIncomingMessageType EmberAfClusterCommand::type
Definition at line
415
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h
source#
EmberNodeId EmberAfClusterCommand::source
Definition at line
416
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h
buffer#
uint8_t* EmberAfClusterCommand::buffer
Definition at line
417
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h
bufLen#
uint16_t EmberAfClusterCommand::bufLen
Definition at line
418
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h
clusterSpecific#
bool EmberAfClusterCommand::clusterSpecific
Definition at line
419
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h
mfgSpecific#
bool EmberAfClusterCommand::mfgSpecific
Definition at line
420
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h
mfgCode#
uint16_t EmberAfClusterCommand::mfgCode
Definition at line
421
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h
seqNum#
uint8_t EmberAfClusterCommand::seqNum
Definition at line
422
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h
commandId#
uint8_t EmberAfClusterCommand::commandId
Definition at line
423
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h
payloadStartIndex#
uint8_t EmberAfClusterCommand::payloadStartIndex
Definition at line
424
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h
direction#
uint8_t EmberAfClusterCommand::direction
Definition at line
425
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h
interPanHeader#
EmberAfInterpanHeader* EmberAfClusterCommand::interPanHeader
Definition at line
426
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h
networkIndex#
uint8_t EmberAfClusterCommand::networkIndex
Definition at line
427
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/include/af-types.h