An in-memory representation of a ZigBee APS frame of an incoming or outgoing message.
Public Attribute Documentation#
profileId#
uint16_t EmberApsFrame::profileId
The application profile ID that describes the format of the message.
clusterId#
uint16_t EmberApsFrame::clusterId
The cluster ID for this message.
sourceEndpoint#
uint8_t EmberApsFrame::sourceEndpoint
The source endpoint.
destinationEndpoint#
uint8_t EmberApsFrame::destinationEndpoint
The destination endpoint.
options#
EmberApsOption EmberApsFrame::options
A bitmask of options from the enumeration above.
groupId#
uint16_t EmberApsFrame::groupId
The group ID for this message, if it is multicast mode.
sequence#
uint8_t EmberApsFrame::sequence
The sequence number.
radius#
uint8_t EmberApsFrame::radius