Defines a result of a network beacon survey.

Public Attributes#

uint16_t
int8_t

Public Attribute Documentation#

nodeId#

uint16_t EmberBeaconSurvey::nodeId

Definition at line 617 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/stack/include/ember-types.h

rssi#

int8_t EmberBeaconSurvey::rssi

Definition at line 618 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/stack/include/ember-types.h

classificationMask#

uint8_t EmberBeaconSurvey::classificationMask

Definition at line 619 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/stack/include/ember-types.h