A structure containing, per device, overall duty cycle consumed (up to the suspend limit).

Public Attribute Documentation#

nodeId#

EmberNodeId EmberPerDeviceDutyCycle::nodeId

Node ID of the device whose duty cycle is reported.


Definition at line 2468 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/stack/include/ember-types.h

dutyCycleConsumed#

EmberDutyCycleHectoPct EmberPerDeviceDutyCycle::dutyCycleConsumed

The amount of overall duty cycle consumed (up to suspend limit).


Definition at line 2470 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/stack/include/ember-types.h