Defines an entry in the binding table.

A binding entry specifies a local endpoint, a remote endpoint, a cluster ID and either the destination EUI64 (for unicast bindings) or the 64-bit group address (for multicast bindings).

Public Attributes#

uint8_t
uint16_t
uint8_t
EmberEUI64

Public Attribute Documentation#

type#

EmberBindingType EmberBindingTableEntry::type

The type of binding.


Definition at line 1281 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/stack/include/ember-types.h

local#

uint8_t EmberBindingTableEntry::local

The endpoint on the local node.


Definition at line 1283 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/stack/include/ember-types.h

clusterId#

uint16_t EmberBindingTableEntry::clusterId

A cluster ID that matches one from the local endpoint's simple descriptor. This cluster ID is set by the provisioning application to indicate which part an endpoint's functionality is bound to this particular remote node and is used to distinguish between unicast and multicast bindings. Note that a binding can be used to to send messages with any cluster ID, not just that listed in the binding.


Definition at line 1291 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/stack/include/ember-types.h

remote#

uint8_t EmberBindingTableEntry::remote

The endpoint on the remote node (specified by identifier).


Definition at line 1293 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/stack/include/ember-types.h

identifier#

EmberEUI64 EmberBindingTableEntry::identifier

A 64-bit identifier. This is either:

  • The destination EUI64, for unicasts.

  • A 16-bit multicast group address, for multicasts.


Definition at line 1298 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/stack/include/ember-types.h

networkIndex#

uint8_t EmberBindingTableEntry::networkIndex

The index of the network the binding belongs to.


Definition at line 1300 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/stack/include/ember-types.h