Holds radio parameters.

This is mainly useful for dual PHY and switched radio device (2.4 Ghz or SubGhz) to retrieve radio parameters.

Public Attributes#

uint8_t

Public Attribute Documentation#

radioTxPower#

int8_t EmberMultiPhyRadioParameters::radioTxPower

Definition at line 1235 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/stack/include/ember-types.h

radioPage#

uint8_t EmberMultiPhyRadioParameters::radioPage

Definition at line 1236 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/stack/include/ember-types.h

radioChannel#

uint8_t EmberMultiPhyRadioParameters::radioChannel

Definition at line 1237 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/stack/include/ember-types.h