BURTC_Init_TypeDef Struct Reference

BURTC initialization structure for Series 2 devices.

#include <em_burtc.h>

Data Fields

bool start
Start BURTC after initialization.
bool debugRun
If true, counter will keep running under debug halt.
uint32_t clkDiv
Clock divider.
bool compare0Top
Set if Compare Value 0 is also top value (counter restart)
bool em4comp
Enable EM4 wakeup on compare match.
bool em4overflow
Enable EM4 wakeup on counter overflow.

BURTC initialization structure for Series 2 devices.

Field Documentation

start

bool BURTC_Init_TypeDef::start

Start BURTC after initialization.

debugRun

bool BURTC_Init_TypeDef::debugRun

If true, counter will keep running under debug halt.

clkDiv

uint32_t BURTC_Init_TypeDef::clkDiv

Clock divider.

Supported range is 1-32768

compare0Top

bool BURTC_Init_TypeDef::compare0Top

Set if Compare Value 0 is also top value (counter restart)

em4comp

bool BURTC_Init_TypeDef::em4comp

Enable EM4 wakeup on compare match.

em4overflow

bool BURTC_Init_TypeDef::em4overflow

Enable EM4 wakeup on counter overflow.