PRS - Peripheral Reflex System

Description

Peripheral Reflex System (PRS) Peripheral API.

This module contains functions to control the PRS peripheral of Silicon Labs 32-bit MCUs and SoCs. The PRS allows configurable, fast, and autonomous communication between peripherals on the MCU or SoC.

Functions

void PRS_SourceSignalSet (unsigned int ch, uint32_t source, uint32_t signal, PRS_Edge_TypeDef edge)
 Set a source and signal for a channel.
 
void PRS_SourceAsyncSignalSet (unsigned int ch, uint32_t source, uint32_t signal)
 Set the source and asynchronous signal for a channel.
 
void PRS_GpioOutputLocation (unsigned int ch, unsigned int location)
 Send the output of a PRS channel to a GPIO pin.
 
int PRS_GetFreeChannel (PRS_ChType_t type)
 Search for the first free PRS channel.
 
void PRS_Reset (void)
 Reset all PRS channels.
 
void PRS_ConnectSignal (unsigned int ch, PRS_ChType_t type, PRS_Signal_t signal)
 Connect a PRS signal to a channel.
 
void PRS_LevelSet (uint32_t level, uint32_t mask)
 Set level control bit for one or more channels.
 
uint32_t PRS_LevelGet (void)
 Get level control bit for all channels.
 
void PRS_PulseTrigger (uint32_t channels)
 Trigger a high pulse (one HFPERCLK) for one or more channels.
 
void PRS_ChannelLevelSet (unsigned int ch, bool level)
 Set the PRS channel level for one asynchronous PRS channel.
 
void PRS_ChannelPulse (unsigned int ch)
 Trigger a pulse on one PRS channel.
 

Macros

#define PRS_SYNC_CHAN_COUNT   PRS_CHAN_COUNT
 PRS Synchronous channel count.
 
#define PRS_ASYNC_CHAN_COUNT   PRS_CHAN_COUNT
 PRS Asynchronous channel count.
 
#define PRS_ASYNC_SUPPORTED   1
 PRS asynchronous support.
 

Enumerations

enum  PRS_ChType_t {
  prsTypeAsync,
  prsTypeSync
}
 PRS Channel type.
 
enum  PRS_Edge_TypeDef {
  prsEdgeOff,
  prsEdgePos,
  prsEdgeNeg,
  prsEdgeBoth
}
 Edge detection type.
 
enum  PRS_Signal_t {
  prsSignalNone = PRS_CH_CTRL_SOURCESEL_NONE | (0x0 << _PRS_CH_CTRL_SIGSEL_SHIFT),
  prsSignalSW = PRS_CH_CTRL_SOURCESEL_NONE | (0x1 << _PRS_CH_CTRL_SIGSEL_SHIFT),
  prsSignalADC0_SINGLE = PRS_ADC0_SINGLE,
  prsSignalADC0_SCAN = PRS_ADC0_SCAN,
  prsSignalTIMER0_UF = PRS_TIMER0_UF,
  prsSignalTIMER0_OF = PRS_TIMER0_OF,
  prsSignalTIMER0_CC0 = PRS_TIMER0_CC0,
  prsSignalTIMER0_CC1 = PRS_TIMER0_CC1,
  prsSignalTIMER0_CC2 = PRS_TIMER0_CC2,
  prsSignalTIMER1_UF = PRS_TIMER1_UF,
  prsSignalTIMER1_OF = PRS_TIMER1_OF,
  prsSignalTIMER1_CC0 = PRS_TIMER1_CC0,
  prsSignalTIMER1_CC1 = PRS_TIMER1_CC1,
  prsSignalTIMER1_CC2 = PRS_TIMER1_CC2,
  prsSignalTIMER2_UF = PRS_TIMER2_UF,
  prsSignalTIMER2_OF = PRS_TIMER2_OF,
  prsSignalTIMER2_CC0 = PRS_TIMER2_CC0,
  prsSignalTIMER2_CC1 = PRS_TIMER2_CC1,
  prsSignalTIMER2_CC2 = PRS_TIMER2_CC2,
  prsSignalTIMER3_UF = PRS_TIMER3_UF,
  prsSignalTIMER3_OF = PRS_TIMER3_OF,
  prsSignalTIMER3_CC0 = PRS_TIMER3_CC0,
  prsSignalTIMER3_CC1 = PRS_TIMER3_CC1,
  prsSignalTIMER3_CC2 = PRS_TIMER3_CC2,
  prsSignalLETIMER0_CH0 = PRS_LETIMER0_CH0,
  prsSignalLETIMER0_CH1 = PRS_LETIMER0_CH1,
  prsSignalRTC_OF = PRS_RTC_OF,
  prsSignalRTC_COMP0 = PRS_RTC_COMP0,
  prsSignalRTC_COMP1 = PRS_RTC_COMP1,
  prsSignalBURTC_COMP = PRS_BURTC_COMP,
  prsSignalBURTC_OF = PRS_BURTC_OF,
  prsSignalACMP0_OUT = PRS_ACMP0_OUT,
  prsSignalACMP1_OUT = PRS_ACMP1_OUT,
  prsSignalLESENSE_SCANRES0 = PRS_LESENSE_SCANRES0,
  prsSignalLESENSE_SCANRES1 = PRS_LESENSE_SCANRES1,
  prsSignalLESENSE_SCANRES2 = PRS_LESENSE_SCANRES2,
  prsSignalLESENSE_SCANRES3 = PRS_LESENSE_SCANRES3,
  prsSignalLESENSE_SCANRES4 = PRS_LESENSE_SCANRES4,
  prsSignalLESENSE_SCANRES5 = PRS_LESENSE_SCANRES5,
  prsSignalLESENSE_SCANRES6 = PRS_LESENSE_SCANRES6,
  prsSignalLESENSE_SCANRES7 = PRS_LESENSE_SCANRES7,
  prsSignalLESENSE_SCANRES8 = PRS_LESENSE_SCANRES8,
  prsSignalLESENSE_SCANRES9 = PRS_LESENSE_SCANRES9,
  prsSignalLESENSE_SCANRES10 = PRS_LESENSE_SCANRES10,
  prsSignalLESENSE_SCANRES11 = PRS_LESENSE_SCANRES11,
  prsSignalLESENSE_SCANRES12 = PRS_LESENSE_SCANRES12,
  prsSignalLESENSE_SCANRES13 = PRS_LESENSE_SCANRES13,
  prsSignalLESENSE_SCANRES14 = PRS_LESENSE_SCANRES14,
  prsSignalLESENSE_SCANRES15 = PRS_LESENSE_SCANRES15,
  prsSignalLESENSE_DEC0 = PRS_LESENSE_DEC0,
  prsSignalLESENSE_DEC1 = PRS_LESENSE_DEC1,
  prsSignalLESENSE_DEC2 = PRS_LESENSE_DEC2,
  prsSignalUSART0_TXC = PRS_USART0_TXC,
  prsSignalUSART0_RXDATAV = PRS_USART0_RXDATAV,
  prsSignalUSART0_IRTX = PRS_USART0_IRTX,
  prsSignalUSART1_TXC = PRS_USART1_TXC,
  prsSignalUSART1_RXDATAV = PRS_USART1_RXDATAV,
  prsSignalUSART2_TXC = PRS_USART2_TXC,
  prsSignalUSART2_RXDATAV = PRS_USART2_RXDATAV,
  prsSignalUART0_TXC = PRS_UART0_TXC,
  prsSignalUART0_RXDATAV = PRS_UART0_RXDATAV,
  prsSignalUART1_TXC = PRS_UART1_TXC,
  prsSignalUART1_RXDATAV = PRS_UART1_RXDATAV,
  prsSignalUSB_SOF = PRS_USB_SOF,
  prsSignalUSB_SOFSR = PRS_USB_SOFSR,
  prsSignalGPIO_PIN0 = PRS_GPIO_PIN0,
  prsSignalGPIO_PIN1 = PRS_GPIO_PIN1,
  prsSignalGPIO_PIN2 = PRS_GPIO_PIN2,
  prsSignalGPIO_PIN3 = PRS_GPIO_PIN3,
  prsSignalGPIO_PIN4 = PRS_GPIO_PIN4,
  prsSignalGPIO_PIN5 = PRS_GPIO_PIN5,
  prsSignalGPIO_PIN6 = PRS_GPIO_PIN6,
  prsSignalGPIO_PIN7 = PRS_GPIO_PIN7,
  prsSignalGPIO_PIN8 = PRS_GPIO_PIN8,
  prsSignalGPIO_PIN9 = PRS_GPIO_PIN9,
  prsSignalGPIO_PIN10 = PRS_GPIO_PIN10,
  prsSignalGPIO_PIN11 = PRS_GPIO_PIN11,
  prsSignalGPIO_PIN12 = PRS_GPIO_PIN12,
  prsSignalGPIO_PIN13 = PRS_GPIO_PIN13,
  prsSignalGPIO_PIN14 = PRS_GPIO_PIN14,
  prsSignalGPIO_PIN15 = PRS_GPIO_PIN15
}
 PRS Signal.
 

Function Documentation

◆ PRS_SourceSignalSet()

void PRS_SourceSignalSet ( unsigned int  ch,
uint32_t  source,
uint32_t  signal,
PRS_Edge_TypeDef  edge 
)

Set a source and signal for a channel.

Parameters
[in]chA channel to define the signal and source for.
[in]sourceA source to select for the channel. Use one of PRS_CH_CTRL_SOURCESEL_x defines.
[in]signalA signal (for selected source) to use. Use one of PRS_CH_CTRL_SIGSEL_x defines.
[in]edgeAn edge (for selected source/signal) to generate the pulse for.

◆ PRS_SourceAsyncSignalSet()

void PRS_SourceAsyncSignalSet ( unsigned int  ch,
uint32_t  source,
uint32_t  signal 
)

Set the source and asynchronous signal for a channel.

Asynchronous reflexes are not clocked on HFPERCLK and can be used even in EM2/EM3. There is a limitation to reflexes operating in asynchronous mode in that they can only be used by a subset of the reflex consumers. See the PRS chapter in the reference manual for the complete list of supported asynchronous signals and consumers.

Note
This function is not supported on EFM32GxxxFyyy parts. In asynchronous mode, the edge detector only works in EM0 and should not be used. The EDSEL parameter in PRS_CHx_CTRL register is set to 0 (OFF) by default.
Parameters
[in]chA channel to define the source and asynchronous signal for.
[in]sourceA source to select for the channel. Use one of PRS_CH_CTRL_SOURCESEL_x defines.
[in]signalAn asynchronous signal (for selected source) to use. Use one of the PRS_CH_CTRL_SIGSEL_x defines that support asynchronous operation.

◆ PRS_GpioOutputLocation()

void PRS_GpioOutputLocation ( unsigned int  ch,
unsigned int  location 
)

Send the output of a PRS channel to a GPIO pin.

This function is used to send the output of a PRS channel to a GPIO pin. Note that there are certain restrictions to where a PRS channel can be routed. Consult the datasheet of the device to see if a channel can be routed to the requested GPIO pin.

Parameters
[in]chPRS channel number.
[in]locationPRS routing location.

◆ PRS_GetFreeChannel()

int PRS_GetFreeChannel ( PRS_ChType_t  type)

Search for the first free PRS channel.

Parameters
[in]typePRS channel type. This can be either prsTypeAsync or prsTypeSync.
Returns
Channel number >= 0 if an unused PRS channel was found. If no free PRS channel was found then -1 is returned.

◆ PRS_Reset()

void PRS_Reset ( void  )

Reset all PRS channels.

This function will reset all the PRS channel configuration.

◆ PRS_ConnectSignal()

void PRS_ConnectSignal ( unsigned int  ch,
PRS_ChType_t  type,
PRS_Signal_t  signal 
)

Connect a PRS signal to a channel.

This function will make the PRS signal available on the specific channel. Only a single PRS signal can be connected to any given channel.

Parameters
[in]chPRS channel number.
[in]typePRS channel type. This can be either prsTypeAsync or prsTypeSync.
[in]signalThis is the PRS signal that should be placed on the channel.

◆ PRS_LevelSet()

void PRS_LevelSet ( uint32_t  level,
uint32_t  mask 
)
inline

Set level control bit for one or more channels.

The level value for a channel is XORed with both the pulse possibly issued by PRS_PulseTrigger() and the PRS input signal selected for the channel(s).

Parameters
[in]levelLevel to use for channels indicated by mask. Use logical OR combination of PRS_SWLEVEL_CHnLEVEL defines for channels to set high level, otherwise 0.
[in]maskMask indicating which channels to set level for. Use logical OR combination of PRS_SWLEVEL_CHnLEVEL defines.

◆ PRS_LevelGet()

uint32_t PRS_LevelGet ( void  )
inline

Get level control bit for all channels.

Returns
The current software level configuration.

◆ PRS_PulseTrigger()

void PRS_PulseTrigger ( uint32_t  channels)
inline

Trigger a high pulse (one HFPERCLK) for one or more channels.

Setting a bit for a channel causes the bit in the register to remain high for one HFPERCLK cycle. Pulse is XORed with both the corresponding bit in PRS SWLEVEL register and the PRS input signal selected for the channel(s).

Parameters
[in]channelsLogical ORed combination of channels to trigger a pulse for. Use PRS_SWPULSE_CHnPULSE defines.

◆ PRS_ChannelLevelSet()

void PRS_ChannelLevelSet ( unsigned int  ch,
bool  level 
)
inline

Set the PRS channel level for one asynchronous PRS channel.

Parameters
[in]chPRS channel number.
[in]leveltrue to set the level high (1) and false to set the level low (0).

◆ PRS_ChannelPulse()

void PRS_ChannelPulse ( unsigned int  ch)
inline

Trigger a pulse on one PRS channel.

Parameters
[in]chPRS channel number.

Macro Definition Documentation

◆ PRS_SYNC_CHAN_COUNT

#define PRS_SYNC_CHAN_COUNT   PRS_CHAN_COUNT

PRS Synchronous channel count.

◆ PRS_ASYNC_CHAN_COUNT

#define PRS_ASYNC_CHAN_COUNT   PRS_CHAN_COUNT

PRS Asynchronous channel count.

◆ PRS_ASYNC_SUPPORTED

#define PRS_ASYNC_SUPPORTED   1

PRS asynchronous support.

Enumeration Type Documentation

◆ PRS_ChType_t

PRS Channel type.

Enumerator
prsTypeAsync 

Asynchronous channel type.

prsTypeSync 

Synchronous channel type.

◆ PRS_Edge_TypeDef

Edge detection type.

Enumerator
prsEdgeOff 

Leave signal as is.

prsEdgePos 

Generate pulses on positive edge.

prsEdgeNeg 

Generate pulses on negative edge.

prsEdgeBoth 

Generate pulses on both edges.

◆ PRS_Signal_t

PRS Signal.

Enumerator
prsSignalNone 

No Signal.

prsSignalSW 

Software-reserved Signal.

prsSignalADC0_SINGLE 

ADC0_SINGLE signal.

prsSignalADC0_SCAN 

ADC0_SCAN signal.

prsSignalTIMER0_UF 

TIMER0 underflow Signal.

prsSignalTIMER0_OF 

TIMER0 overflow Signal.

prsSignalTIMER0_CC0 

TIMER0 capture/compare channel 0 Signal.

prsSignalTIMER0_CC1 

TIMER0 capture/compare channel 1 Signal.

prsSignalTIMER0_CC2 

TIMER0 capture/compare channel 2 Signal.

prsSignalTIMER1_UF 

TIMER1 underflow Signal.

prsSignalTIMER1_OF 

TIMER1 overflow Signal.

prsSignalTIMER1_CC0 

TIMER1 capture/compare channel 0 Signal.

prsSignalTIMER1_CC1 

TIMER1 capture/compare channel 1 Signal.

prsSignalTIMER1_CC2 

TIMER1 capture/compare channel 2 Signal.

prsSignalTIMER2_UF 

TIMER2 underflow Signal.

prsSignalTIMER2_OF 

TIMER2 overflow Signal.

prsSignalTIMER2_CC0 

TIMER2 capture/compare channel 0 Signal.

prsSignalTIMER2_CC1 

TIMER2 capture/compare channel 1 Signal.

prsSignalTIMER2_CC2 

TIMER2 capture/compare channel 2 Signal.

prsSignalTIMER3_UF 

TIMER3 underflow Signal.

prsSignalTIMER3_OF 

TIMER3 overflow Signal.

prsSignalTIMER3_CC0 

TIMER3 capture/compare channel 0 Signal.

prsSignalTIMER3_CC1 

TIMER3 capture/compare channel 1 Signal.

prsSignalTIMER3_CC2 

TIMER3 capture/compare channel 2 Signal.

prsSignalLETIMER0_CH0 

LETIMER0 channel 0 Signal.

prsSignalLETIMER0_CH1 

LETIMER0 channel 1 Signal.

prsSignalRTC_OF 

RTC_OF signal.

prsSignalRTC_COMP0 

RTC_COMP0 signal.

prsSignalRTC_COMP1 

RTC_COMP1 signal.

prsSignalBURTC_COMP 

BURTC compare Signal.


prsSignalBURTC_OF 

BURTC overflow Signal.

prsSignalACMP0_OUT 

ACMP0 output Signal.

prsSignalACMP1_OUT 

ACMP1 output Signal.

prsSignalLESENSE_SCANRES0 

LESENSE_SCANRES0 Signal.

prsSignalLESENSE_SCANRES1 

LESENSE_SCANRES1 Signal.

prsSignalLESENSE_SCANRES2 

LESENSE_SCANRES2 Signal.

prsSignalLESENSE_SCANRES3 

LESENSE_SCANRES3 Signal.

prsSignalLESENSE_SCANRES4 

LESENSE_SCANRES4 Signal.

prsSignalLESENSE_SCANRES5 

LESENSE_SCANRES5 Signal.

prsSignalLESENSE_SCANRES6 

LESENSE_SCANRES6 Signal.

prsSignalLESENSE_SCANRES7 

LESENSE_SCANRES7 Signal.

prsSignalLESENSE_SCANRES8 

LESENSE_SCANRES8 Signal.

prsSignalLESENSE_SCANRES9 

LESENSE_SCANRES9 Signal.

prsSignalLESENSE_SCANRES10 

LESENSE_SCANRES10 Signal.

prsSignalLESENSE_SCANRES11 

LESENSE_SCANRES11 Signal.

prsSignalLESENSE_SCANRES12 

LESENSE_SCANRES12 Signal.

prsSignalLESENSE_SCANRES13 

LESENSE_SCANRES13 Signal.

prsSignalLESENSE_SCANRES14 

LESENSE_SCANRES14 Signal.

prsSignalLESENSE_SCANRES15 

LESENSE_SCANRES15 Signal.

prsSignalLESENSE_DEC0 

LESENSE_DEC0 Signal.

prsSignalLESENSE_DEC1 

LESENSE_DEC1 Signal.

prsSignalLESENSE_DEC2 

LESENSE_DEC2 Signal.

prsSignalUSART0_TXC 

USART0 tx complete Signal.

prsSignalUSART0_RXDATAV 

USART0 rx data available Signal.

prsSignalUSART0_IRTX 

USART0 IR tx Signal.

prsSignalUSART1_TXC 

USART1 tx complete Signal.

prsSignalUSART1_RXDATAV 

USART1 rx data available Signal.

prsSignalUSART2_TXC 

USART2 tx complete Signal.

prsSignalUSART2_RXDATAV 

USART2 rx data available Signal.

prsSignalUART0_TXC 

UART0 tx complete Signal.

prsSignalUART0_RXDATAV 

UART0 rx data available Signal.

prsSignalUART1_TXC 

UART1 tx complete Signal.

prsSignalUART1_RXDATAV 

UART1 rx data available Signal.

prsSignalUSB_SOF 

USB_SOF Signal.

prsSignalUSB_SOFSR 

USB_SOFSR Signal.

prsSignalGPIO_PIN0 

GPIO Pin 0 Signal.

prsSignalGPIO_PIN1 

GPIO Pin 1 Signal.

prsSignalGPIO_PIN2 

GPIO Pin 2 Signal.

prsSignalGPIO_PIN3 

GPIO Pin 3 Signal.

prsSignalGPIO_PIN4 

GPIO Pin 4 Signal.

prsSignalGPIO_PIN5 

GPIO Pin 5 Signal.

prsSignalGPIO_PIN6 

GPIO Pin 6 Signal.

prsSignalGPIO_PIN7 

GPIO Pin 7 Signal.

prsSignalGPIO_PIN8 

GPIO Pin 8 Signal.

prsSignalGPIO_PIN9 

GPIO Pin 9 Signal.

prsSignalGPIO_PIN10 

GPIO Pin 10 Signal.

prsSignalGPIO_PIN11 

GPIO Pin 11 Signal.

prsSignalGPIO_PIN12 

GPIO Pin 12 Signal.

prsSignalGPIO_PIN13 

GPIO Pin 13 Signal.

prsSignalGPIO_PIN14 

GPIO Pin 14 Signal.

prsSignalGPIO_PIN15 

GPIO Pin 15 Signal.