Description

Secure Element key handling API.

API for using cryptographic keys with the SE. Contains functionality to generate, import and export keys to and from protected types like wrapped or volatile keys.

Data Structures

struct  sl_se_buffer_t
 Describes where the key is or should be stored.
 
struct  sl_se_key_storage_t
 Describes the storage location of keys.
 
struct  sl_se_key_descriptor_t
 Contains a full description of a key used by an SE command.
 
struct  sl_se_custom_weierstrass_prime_domain_t
 Custom Weierstrass curve structure.
 

Functions

sl_status_t sl_se_validate_key (const sl_se_key_descriptor_t *key)
 Validate key descriptor.
 
sl_status_t sl_se_generate_key (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key_out)
 Generate a random key adhering to the given key descriptor.
 
sl_status_t sl_se_import_key (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key_in, const sl_se_key_descriptor_t *key_out)
 Import a key using the SE.
 
sl_status_t sl_se_export_key (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key_in, const sl_se_key_descriptor_t *key_out)
 Export a volatile or wrapped key back to plaintext.
 
sl_status_t sl_se_transfer_key (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key_in, const sl_se_key_descriptor_t *key_out)
 Transfer a volatile or wrapped key to another protected storage.
 
sl_status_t sl_se_export_public_key (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key_in, const sl_se_key_descriptor_t *key_out)
 Export the public part of an ECC keypair.
 
sl_status_t sl_se_delete_key (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key)
 Delete a key from a volatile SE storage slot.
 
sl_status_t sl_se_get_storage_size (const sl_se_key_descriptor_t *key, uint32_t *storage_size)
 Returns the required storage size for the given key.
 

Macros

#define SL_SE_KEY_FLAG_ASYMMETRIC_SIGNING_ONLY   (1UL << 10)
 Asymmetric key can only be used for signing (not key exchange)
 
#define SL_SE_KEY_FLAG_ASYMMETRIC_USES_CUSTOM_DOMAIN   (1UL << 12)
 Described key belongs to a custom ECC domain.
 
#define SL_SE_KEY_FLAG_ASYMMETRIC_BUFFER_HAS_PUBLIC_KEY   (1UL << 13)
 Storage buffer contains public part of an asymmetric key.
 
#define SL_SE_KEY_FLAG_ASYMMETRIC_BUFFER_HAS_PRIVATE_KEY   (1UL << 14)
 Storage buffer contains private part of an asymmetric key.
 
#define SL_SE_KEY_FLAG_ALLOW_ANY_ACCESS   (1UL << 15)
 Allow usage of this key by other bus masters or TrustZone levels than the one which created/imported the key.
 
#define SL_SE_KEY_FLAG_ASYMMMETRIC_SIGNING_ONLY   (SL_SE_KEY_FLAG_ASYMMETRIC_SIGNING_ONLY)
 Old definition. Retained for backwards compatibility.
 
#define SL_SE_KEY_FLAG_NON_EXPORTABLE   (1UL << 24)
 Do not allow exporting the key to plaintext.
 
#define SL_SE_KEY_FLAG_IS_DEVICE_GENERATED   (1UL << 25)
 Indicate that the key has been generated by this device.
 
#define SL_SE_KEY_FLAG_IS_RESTRICTED   (1UL << 25 | 1UL << 24)
 Indicate that the key can only be used to sign SE generated content.
 
#define SL_SE_KEY_TYPE_ALGORITHM_MASK   0xf0000000
 Mask for algorithm field in key type.
 
#define SL_SE_KEY_TYPE_ALGORITHM_OFFSET   28
 Offset of algorithm field in key type.
 
#define SL_SE_KEY_TYPE_ATTRIBUTES_MASK   0x00007fff
 Mask for attributes field in key type.
 
#define SL_SE_KEY_TYPE_ATTRIBUTES_OFFSET   0
 Offset of attributes field in key type.
 
#define SL_SE_KEY_TYPE_SYMMETRIC   0x00000000
 Symmetric key type.
 
#define SL_SE_KEY_TYPE_AES_128   0x00000010
 Symmetric key type for AES-128 (16 byte key)
 
#define SL_SE_KEY_TYPE_AES_192   0x00000018
 Symmetric key type for AES-192 (24 byte key)
 
#define SL_SE_KEY_TYPE_AES_256   0x00000020
 Symmetric key type for AES-256 (32 byte key)
 
#define SL_SE_KEY_TYPE_ECC_WEIERSTRASS_PRIME_CUSTOM   (0x8U << SL_SE_KEY_TYPE_ALGORITHM_OFFSET)
 ECC Weierstrass Prime key type.
 
#define SL_SE_KEY_TYPE_ECC_P192   (SL_SE_KEY_TYPE_ECC_WEIERSTRASS_PRIME_CUSTOM | (0x18))
 ECC NIST P-192.
 
#define SL_SE_KEY_TYPE_ECC_P256   (SL_SE_KEY_TYPE_ECC_WEIERSTRASS_PRIME_CUSTOM | (0x20))
 ECC NIST P-256.
 
#define SL_SE_KEY_TYPE_CHACHA20   0x00000020
 Symmetric key type for ChaCha20.
 
#define SL_SE_KEY_TYPE_ECC_MONTGOMERY   (0xbU << SL_SE_KEY_TYPE_ALGORITHM_OFFSET)
 ECC Montgomery key type.
 
#define SL_SE_KEY_TYPE_ECC_EDDSA   (0xcU << SL_SE_KEY_TYPE_ALGORITHM_OFFSET)
 EDDSA key type.
 
#define SL_SE_KEY_TYPE_ECC_P384   (SL_SE_KEY_TYPE_ECC_WEIERSTRASS_PRIME_CUSTOM | (0x30))
 ECC NIST P-384.
 
#define SL_SE_KEY_TYPE_ECC_P521   (SL_SE_KEY_TYPE_ECC_WEIERSTRASS_PRIME_CUSTOM | (0x42))
 ECC NIST P-521.
 
#define SL_SE_KEY_TYPE_ECC_X25519   (SL_SE_KEY_TYPE_ECC_MONTGOMERY | (0x20))
 ECC X25519 key for ECDH.
 
#define SL_SE_KEY_TYPE_ECC_X448   (SL_SE_KEY_TYPE_ECC_MONTGOMERY | (0x38))
 ECC X448 key for ECDH.
 
#define SL_SE_KEY_STORAGE_EXTERNAL_PLAINTEXT   0x00
 Key storage methods.
 
#define SL_SE_KEY_STORAGE_EXTERNAL_WRAPPED   0x01
 Key is stored encrypted in application memory.
 
#define SL_SE_KEY_STORAGE_INTERNAL_VOLATILE   0x02
 Key is stored inside the SE, and will persist until system reset or explicitly deleted.
 
#define SL_SE_KEY_STORAGE_INTERNAL_IMMUTABLE   0x03
 Key is one of the pre-defined keys (pre-loaded or write-once) available in the SE.
 
#define SL_SE_KEY_SLOT_VOLATILE_0   0x00
 List of available internal SE key slots.
 
#define SL_SE_KEY_SLOT_VOLATILE_1   0x01
 Internal volatile slot 1.
 
#define SL_SE_KEY_SLOT_VOLATILE_2   0x02
 Internal volatile slot 2.
 
#define SL_SE_KEY_SLOT_VOLATILE_3   0x03
 Internal volatile slot 3.
 
#define SL_SE_KEY_SLOT_APPLICATION_SECURE_DEBUG_KEY   0xF8
 Internal immutable application secure debug key.
 
#define SL_SE_KEY_SLOT_APPLICATION_AES_128_KEY   0xFA
 Internal immutable application AES-128 key (bootloader key)
 
#define SL_SE_KEY_SLOT_APPLICATION_SECURE_BOOT_KEY   0xFC
 Internal immutable application secure boot key.
 
#define SL_SE_KEY_SLOT_APPLICATION_ATTESTATION_KEY   0xFE
 Internal immutable application attestation key.
 
#define SL_SE_KEY_SLOT_SE_ATTESTATION_KEY   0xFF
 Internal immutable SE attestation key.
 
#define SLI_SE_WRAPPED_KEY_OVERHEAD   (12 + 16)
 Size overhead for wrapped keys.
 

Typedefs

typedef uint32_t sl_se_key_type_t
 Supported key types.
 
typedef uint32_t sl_se_storage_method_t
 Key storage method.
 
typedef uint32_t sl_se_key_slot_t
 Internal SE key slot.
 

Function Documentation

◆ sl_se_validate_key()

sl_status_t sl_se_validate_key ( const sl_se_key_descriptor_t key)

Validate key descriptor.

Takes a key descriptor and checks if all required properties have been set for the specific key type.

Parameters
[in]keyThe key to validate.
Returns
Status code, sl_status.h.

◆ sl_se_generate_key()

sl_status_t sl_se_generate_key ( sl_se_command_context_t cmd_ctx,
const sl_se_key_descriptor_t key_out 
)

Generate a random key adhering to the given key descriptor.

The SE takes a key descriptor and generates a key with the given properties in the location specified by the descriptor.

If the key size is not aligned to a multiple of words the key representation is padded in front of the key.

Parameters
[in]cmd_ctxPointer to an SE command context object.
[in]key_outDescription of the key to generate. Sets key parameters and describes the storage location for the key.
Returns
Status code, sl_status.h.

◆ sl_se_import_key()

sl_status_t sl_se_import_key ( sl_se_command_context_t cmd_ctx,
const sl_se_key_descriptor_t key_in,
const sl_se_key_descriptor_t key_out 
)

Import a key using the SE.

Protect a key using the SE. Import a plaintext key and store it either in a volatile slot or as a wrapped key.

Parameters
[in]cmd_ctxPointer to an SE command context object.
[in]key_inA plaintext key.
[in]key_outEither a volatile or a wrapped key with similar properties as key_in.
Returns
Status code, sl_status.h.

◆ sl_se_export_key()

sl_status_t sl_se_export_key ( sl_se_command_context_t cmd_ctx,
const sl_se_key_descriptor_t key_in,
const sl_se_key_descriptor_t key_out 
)

Export a volatile or wrapped key back to plaintext.

Attempt to have the SE export a volatile or wrapped key back to plaintext if allowed.

Parameters
[in]cmd_ctxPointer to an SE command context object.
[in]key_inEither a volatile or a wrapped key with similar properties as key_out.
[in]key_outThe exported key in plaintext.
Returns
Status code, sl_status.h. SL_STATUS_INVALID_PARAMETER if key does not exist.

◆ sl_se_transfer_key()

sl_status_t sl_se_transfer_key ( sl_se_command_context_t cmd_ctx,
const sl_se_key_descriptor_t key_in,
const sl_se_key_descriptor_t key_out 
)

Transfer a volatile or wrapped key to another protected storage.

Attempt to have the SE transfer a volatile or wrapped key if allowed.

Note
The key stored in the source protected storage will not be deleted.

Transferring a key between the same volatile slot is not allowed.

Parameters
[in]cmd_ctxPointer to an SE command context object.
[in]key_inEither a volatile or a wrapped key with similar properties as key_out.
[in]key_outEither a volatile or a wrapped key with similar properties as key_in.
Returns
Status code, sl_status.h. SL_STATUS_INVALID_PARAMETER if key does not exist.

◆ sl_se_export_public_key()

sl_status_t sl_se_export_public_key ( sl_se_command_context_t cmd_ctx,
const sl_se_key_descriptor_t key_in,
const sl_se_key_descriptor_t key_out 
)

Export the public part of an ECC keypair.

The output key must be specified to only contain a public key.

Parameters
[in]cmd_ctxPointer to an SE command context object.
[in]key_inAn asymmetric key with either a private or public part.
[out]key_outDescribes output key parameters. Should only be set to contain the public part of the key.
Returns
Status code, sl_status.h.

◆ sl_se_delete_key()

sl_status_t sl_se_delete_key ( sl_se_command_context_t cmd_ctx,
const sl_se_key_descriptor_t key 
)

Delete a key from a volatile SE storage slot.

The given key will be removed from the SE. The key descriptor is not modified and can be used to generate a new key without any updates.

Parameters
[in]cmd_ctxPointer to an SE command context object.
[in]keyKey to delete.
Returns
Status code, sl_status.h.

◆ sl_se_get_storage_size()

sl_status_t sl_se_get_storage_size ( const sl_se_key_descriptor_t key,
uint32_t *  storage_size 
)

Returns the required storage size for the given key.

Finds the total storage size required for a given key. This includes storage for the public and private part of asymmetric keys, as well as overhead for wrapping keys.

Parameters
[in]keyThe sl_se_key_descriptor_t to find the required storage size for.
[out]storage_sizeThe required storage size in bytes.
Returns
Status code, sl_status.h.

Macro Definition Documentation

◆ SL_SE_KEY_FLAG_ASYMMETRIC_SIGNING_ONLY

#define SL_SE_KEY_FLAG_ASYMMETRIC_SIGNING_ONLY   (1UL << 10)

Asymmetric key can only be used for signing (not key exchange)

◆ SL_SE_KEY_FLAG_ASYMMETRIC_USES_CUSTOM_DOMAIN

#define SL_SE_KEY_FLAG_ASYMMETRIC_USES_CUSTOM_DOMAIN   (1UL << 12)

Described key belongs to a custom ECC domain.

◆ SL_SE_KEY_FLAG_ASYMMETRIC_BUFFER_HAS_PUBLIC_KEY

#define SL_SE_KEY_FLAG_ASYMMETRIC_BUFFER_HAS_PUBLIC_KEY   (1UL << 13)

Storage buffer contains public part of an asymmetric key.

◆ SL_SE_KEY_FLAG_ASYMMETRIC_BUFFER_HAS_PRIVATE_KEY

#define SL_SE_KEY_FLAG_ASYMMETRIC_BUFFER_HAS_PRIVATE_KEY   (1UL << 14)

Storage buffer contains private part of an asymmetric key.

◆ SL_SE_KEY_FLAG_ALLOW_ANY_ACCESS

#define SL_SE_KEY_FLAG_ALLOW_ANY_ACCESS   (1UL << 15)

Allow usage of this key by other bus masters or TrustZone levels than the one which created/imported the key.

◆ SL_SE_KEY_FLAG_ASYMMMETRIC_SIGNING_ONLY

#define SL_SE_KEY_FLAG_ASYMMMETRIC_SIGNING_ONLY   (SL_SE_KEY_FLAG_ASYMMETRIC_SIGNING_ONLY)

Old definition. Retained for backwards compatibility.

◆ SL_SE_KEY_FLAG_NON_EXPORTABLE

#define SL_SE_KEY_FLAG_NON_EXPORTABLE   (1UL << 24)

Do not allow exporting the key to plaintext.

◆ SL_SE_KEY_FLAG_IS_DEVICE_GENERATED

#define SL_SE_KEY_FLAG_IS_DEVICE_GENERATED   (1UL << 25)

Indicate that the key has been generated by this device.

This flag is only valid when using the SE to generate a key and makes it non-exportable.

◆ SL_SE_KEY_FLAG_IS_RESTRICTED

#define SL_SE_KEY_FLAG_IS_RESTRICTED   (1UL << 25 | 1UL << 24)

Indicate that the key can only be used to sign SE generated content.

This flag is only valid when using the SE to generate a key and makes it non-exportable.

◆ SL_SE_KEY_TYPE_ALGORITHM_MASK

#define SL_SE_KEY_TYPE_ALGORITHM_MASK   0xf0000000

Mask for algorithm field in key type.

◆ SL_SE_KEY_TYPE_ALGORITHM_OFFSET

#define SL_SE_KEY_TYPE_ALGORITHM_OFFSET   28

Offset of algorithm field in key type.

◆ SL_SE_KEY_TYPE_ATTRIBUTES_MASK

#define SL_SE_KEY_TYPE_ATTRIBUTES_MASK   0x00007fff

Mask for attributes field in key type.

◆ SL_SE_KEY_TYPE_ATTRIBUTES_OFFSET

#define SL_SE_KEY_TYPE_ATTRIBUTES_OFFSET   0

Offset of attributes field in key type.

◆ SL_SE_KEY_TYPE_SYMMETRIC

#define SL_SE_KEY_TYPE_SYMMETRIC   0x00000000

Symmetric key type.

◆ SL_SE_KEY_TYPE_AES_128

#define SL_SE_KEY_TYPE_AES_128   0x00000010

Symmetric key type for AES-128 (16 byte key)

◆ SL_SE_KEY_TYPE_AES_192

#define SL_SE_KEY_TYPE_AES_192   0x00000018

Symmetric key type for AES-192 (24 byte key)

◆ SL_SE_KEY_TYPE_AES_256

#define SL_SE_KEY_TYPE_AES_256   0x00000020

Symmetric key type for AES-256 (32 byte key)

◆ SL_SE_KEY_TYPE_ECC_WEIERSTRASS_PRIME_CUSTOM

#define SL_SE_KEY_TYPE_ECC_WEIERSTRASS_PRIME_CUSTOM   (0x8U << SL_SE_KEY_TYPE_ALGORITHM_OFFSET)

ECC Weierstrass Prime key type.

◆ SL_SE_KEY_TYPE_ECC_P192

#define SL_SE_KEY_TYPE_ECC_P192   (SL_SE_KEY_TYPE_ECC_WEIERSTRASS_PRIME_CUSTOM | (0x18))

ECC NIST P-192.

◆ SL_SE_KEY_TYPE_ECC_P256

#define SL_SE_KEY_TYPE_ECC_P256   (SL_SE_KEY_TYPE_ECC_WEIERSTRASS_PRIME_CUSTOM | (0x20))

ECC NIST P-256.

◆ SL_SE_KEY_TYPE_CHACHA20

#define SL_SE_KEY_TYPE_CHACHA20   0x00000020

Symmetric key type for ChaCha20.

◆ SL_SE_KEY_TYPE_ECC_MONTGOMERY

#define SL_SE_KEY_TYPE_ECC_MONTGOMERY   (0xbU << SL_SE_KEY_TYPE_ALGORITHM_OFFSET)

ECC Montgomery key type.

◆ SL_SE_KEY_TYPE_ECC_EDDSA

#define SL_SE_KEY_TYPE_ECC_EDDSA   (0xcU << SL_SE_KEY_TYPE_ALGORITHM_OFFSET)

EDDSA key type.

◆ SL_SE_KEY_TYPE_ECC_P384

#define SL_SE_KEY_TYPE_ECC_P384   (SL_SE_KEY_TYPE_ECC_WEIERSTRASS_PRIME_CUSTOM | (0x30))

ECC NIST P-384.

◆ SL_SE_KEY_TYPE_ECC_P521

#define SL_SE_KEY_TYPE_ECC_P521   (SL_SE_KEY_TYPE_ECC_WEIERSTRASS_PRIME_CUSTOM | (0x42))

ECC NIST P-521.

◆ SL_SE_KEY_TYPE_ECC_X25519

#define SL_SE_KEY_TYPE_ECC_X25519   (SL_SE_KEY_TYPE_ECC_MONTGOMERY | (0x20))

ECC X25519 key for ECDH.

◆ SL_SE_KEY_TYPE_ECC_X448

#define SL_SE_KEY_TYPE_ECC_X448   (SL_SE_KEY_TYPE_ECC_MONTGOMERY | (0x38))

ECC X448 key for ECDH.

◆ SL_SE_KEY_STORAGE_EXTERNAL_PLAINTEXT

#define SL_SE_KEY_STORAGE_EXTERNAL_PLAINTEXT   0x00

Key storage methods.

Key is stored in a plaintext buffer in application memory. Application can save its in-memory buffer to non-volatile memory as needed to provide key persistence.

◆ SL_SE_KEY_STORAGE_EXTERNAL_WRAPPED

#define SL_SE_KEY_STORAGE_EXTERNAL_WRAPPED   0x01

Key is stored encrypted in application memory.

This ensures the key in wrapped form is only usable on a specific device. If the key additionally needs to be prevented from ever being output as plaintext, also set the corresponding permission bit. Application can save its in-memory buffer to non-volatile memory as needed to provide key persistence. Keys stored in this way should use the flag SL_SE_KEY_FLAG_NON_EXPORTABLE unless there is a specific need to access the key value outside the SE.

◆ SL_SE_KEY_STORAGE_INTERNAL_VOLATILE

#define SL_SE_KEY_STORAGE_INTERNAL_VOLATILE   0x02

Key is stored inside the SE, and will persist until system reset or explicitly deleted.

Keys stored in this way should use the flag SL_SE_KEY_FLAG_NON_EXPORTABLE unless there is a specific need to access the key value outside the SE.

◆ SL_SE_KEY_STORAGE_INTERNAL_IMMUTABLE

#define SL_SE_KEY_STORAGE_INTERNAL_IMMUTABLE   0x03

Key is one of the pre-defined keys (pre-loaded or write-once) available in the SE.

See documentation for a list of available keys.

◆ SL_SE_KEY_SLOT_VOLATILE_0

#define SL_SE_KEY_SLOT_VOLATILE_0   0x00

List of available internal SE key slots.

Internal volatile slot 0

◆ SL_SE_KEY_SLOT_VOLATILE_1

#define SL_SE_KEY_SLOT_VOLATILE_1   0x01

Internal volatile slot 1.

◆ SL_SE_KEY_SLOT_VOLATILE_2

#define SL_SE_KEY_SLOT_VOLATILE_2   0x02

Internal volatile slot 2.

◆ SL_SE_KEY_SLOT_VOLATILE_3

#define SL_SE_KEY_SLOT_VOLATILE_3   0x03

Internal volatile slot 3.

◆ SL_SE_KEY_SLOT_APPLICATION_SECURE_DEBUG_KEY

#define SL_SE_KEY_SLOT_APPLICATION_SECURE_DEBUG_KEY   0xF8

Internal immutable application secure debug key.

◆ SL_SE_KEY_SLOT_APPLICATION_AES_128_KEY

#define SL_SE_KEY_SLOT_APPLICATION_AES_128_KEY   0xFA

Internal immutable application AES-128 key (bootloader key)

◆ SL_SE_KEY_SLOT_APPLICATION_SECURE_BOOT_KEY

#define SL_SE_KEY_SLOT_APPLICATION_SECURE_BOOT_KEY   0xFC

Internal immutable application secure boot key.

◆ SL_SE_KEY_SLOT_APPLICATION_ATTESTATION_KEY

#define SL_SE_KEY_SLOT_APPLICATION_ATTESTATION_KEY   0xFE

Internal immutable application attestation key.

◆ SL_SE_KEY_SLOT_SE_ATTESTATION_KEY

#define SL_SE_KEY_SLOT_SE_ATTESTATION_KEY   0xFF

Internal immutable SE attestation key.

◆ SLI_SE_WRAPPED_KEY_OVERHEAD

#define SLI_SE_WRAPPED_KEY_OVERHEAD   (12 + 16)

Size overhead for wrapped keys.

Typedef Documentation

◆ sl_se_key_type_t

typedef uint32_t sl_se_key_type_t

Supported key types.

◆ sl_se_storage_method_t

◆ sl_se_key_slot_t

typedef uint32_t sl_se_key_slot_t

Internal SE key slot.