BMP_Header Struct Reference
BMP Module header structure.
#include <bmp.h>
Data Fields | |
uint16_t | magic |
Magic identifier: "BM" (for bmp files) | |
uint32_t | fileSize |
Size of the bmp file in bytes. | |
uint16_t | reserved1 |
Reserved 1. | |
uint16_t | reserved2 |
Reserved 2. | |
uint32_t | dataOffset |
Data offset relative to the start of the bmp data. | |
uint32_t | headerSize |
Header size in bytes. | |
uint32_t | width |
Width of bmp. | |
uint32_t | height |
Height of bmp. | |
uint16_t | colorPlanes |
Color planes. | |
uint16_t | bitsPerPixel |
Color depth. | |
uint32_t | compressionType |
Compression type. | |
uint32_t | imageDataSize |
Size of raw BMP data. | |
uint32_t | hPixelsPerMeter |
Horizontal resolution (pixels per meter) | |
uint32_t | vPixelsPerMeter |
Vertical resolution (pixels per meter) | |
uint32_t | colorsUsed |
Number of color indices in the color table that are actually used by the bitmap. | |
uint32_t | colorsRequired |
Number of color indices that are required for displaying the bitmap. | |
BMP Module header structure.
Must be packed to exact 54 bytes.
Field Documentation
◆ magic
uint16_t BMP_Header::magic |
Magic identifier: "BM" (for bmp files)
◆ fileSize
uint32_t BMP_Header::fileSize |
Size of the bmp file in bytes.
◆ reserved1
uint16_t BMP_Header::reserved1 |
Reserved 1.
◆ reserved2
uint16_t BMP_Header::reserved2 |
Reserved 2.
◆ dataOffset
uint32_t BMP_Header::dataOffset |
Data offset relative to the start of the bmp data.
◆ headerSize
uint32_t BMP_Header::headerSize |
Header size in bytes.
◆ width
uint32_t BMP_Header::width |
Width of bmp.
◆ height
uint32_t BMP_Header::height |
Height of bmp.
◆ colorPlanes
uint16_t BMP_Header::colorPlanes |
Color planes.
◆ bitsPerPixel
uint16_t BMP_Header::bitsPerPixel |
Color depth.
◆ compressionType
uint32_t BMP_Header::compressionType |
Compression type.
◆ imageDataSize
uint32_t BMP_Header::imageDataSize |
Size of raw BMP data.
◆ hPixelsPerMeter
uint32_t BMP_Header::hPixelsPerMeter |
Horizontal resolution (pixels per meter)
◆ vPixelsPerMeter
uint32_t BMP_Header::vPixelsPerMeter |
Vertical resolution (pixels per meter)
◆ colorsUsed
uint32_t BMP_Header::colorsUsed |
Number of color indices in the color table that are actually used by the bitmap.
◆ colorsRequired
uint32_t BMP_Header::colorsRequired |
Number of color indices that are required for displaying the bitmap.