sl_se_key_descriptor_t Struct Reference
Contains a full description of a key used by an SE command.
#include <sl_se_manager_types.h>
Data Fields | |
sl_se_key_type_t | type |
Key type. | |
size_t | size |
Key size, applicable if key_type == SYMMETRIC. | |
uint32_t | flags |
Flags describing restrictions, permissions and attributes of the key. | |
sl_se_key_storage_t | storage |
Storage location for this key. | |
uint8_t * | password |
Optional password for key usage (8 bytes). | |
const void * | domain |
Pointer to domain descriptor if this key contains an asymmetric key on a custom domain The reason for pointing instead of containing is to make it possible to have the parameters in ROM. | |
Contains a full description of a key used by an SE command.
Field Documentation
◆ type
sl_se_key_type_t sl_se_key_descriptor_t::type |
Key type.
◆ size
size_t sl_se_key_descriptor_t::size |
Key size, applicable if key_type == SYMMETRIC.
◆ flags
uint32_t sl_se_key_descriptor_t::flags |
Flags describing restrictions, permissions and attributes of the key.
◆ storage
sl_se_key_storage_t sl_se_key_descriptor_t::storage |
Storage location for this key.
◆ password
uint8_t* sl_se_key_descriptor_t::password |
Optional password for key usage (8 bytes).
If no password is provided (NULL pointer), any key not stored as plaintext will be stored with a password of all-zero bytes.
◆ domain
const void* sl_se_key_descriptor_t::domain |
Pointer to domain descriptor if this key contains an asymmetric key on a custom domain The reason for pointing instead of containing is to make it possible to have the parameters in ROM.