DAC - Digital to Analog Converter
Description
Digital to Analog Converter (DAC) Peripheral API.
This module contains functions to control the DAC peripheral of Silicon Labs 32-bit MCUs and SoCs. The DAC converts digital values to analog signals at up to 500 ksps with 12-bit accuracy. The DAC is designed for low-energy consumption and can also provide very good performance.
| Data Structures | |
| struct | DAC_Init_TypeDef | 
| DAC initialization structure, common for both channels. | |
| struct | DAC_InitChannel_TypeDef | 
| DAC channel initialization structure. | |
| Functions | |
| void | DAC_Enable (DAC_TypeDef *dac, unsigned int ch, bool enable) | 
| Enable/disable the DAC channel. | |
| void | DAC_Init (DAC_TypeDef *dac, const DAC_Init_TypeDef *init) | 
| Initialize DAC. | |
| void | DAC_InitChannel (DAC_TypeDef *dac, const DAC_InitChannel_TypeDef *init, unsigned int ch) | 
| Initialize DAC channel. | |
| void | DAC_ChannelOutputSet (DAC_TypeDef *dac, unsigned int channel, uint32_t value) | 
| Set the output signal of a DAC channel to a given value. | |
| void | DAC_Channel0OutputSet (DAC_TypeDef *dac, uint32_t value) | 
| Set the output signal of DAC channel 0 to a given value. | |
| void | DAC_Channel1OutputSet (DAC_TypeDef *dac, uint32_t value) | 
| Set the output signal of DAC channel 1 to a given value. | |
| void | DAC_IntClear (DAC_TypeDef *dac, uint32_t flags) | 
| Clear one or more pending DAC interrupts. | |
| void | DAC_IntDisable (DAC_TypeDef *dac, uint32_t flags) | 
| Disable one or more DAC interrupts. | |
| void | DAC_IntEnable (DAC_TypeDef *dac, uint32_t flags) | 
| Enable one or more DAC interrupts. | |
| uint32_t | DAC_IntGet (DAC_TypeDef *dac) | 
| Get pending DAC interrupt flags. | |
| uint32_t | DAC_IntGetEnabled (DAC_TypeDef *dac) | 
| Get enabled and pending DAC interrupt flags. | |
| void | DAC_IntSet (DAC_TypeDef *dac, uint32_t flags) | 
| Set one or more pending DAC interrupts from SW. | |
| uint8_t | DAC_PrescaleCalc (uint32_t dacFreq, uint32_t hfperFreq) | 
| Calculate prescaler value used to determine the DAC clock. | |
| void | DAC_Reset (DAC_TypeDef *dac) | 
| Reset DAC to the same state that it was in after a hardware reset. | |
| Macros | |
| #define | DAC_INIT_DEFAULT | 
| Default configuration for DAC initialization structure. | |
| #define | DAC_INITCHANNEL_DEFAULT | 
| Default configuration for DAC channel initialization structure. | |
| Enumerations | |
| enum | DAC_ConvMode_TypeDef
         
         { dacConvModeContinuous = _DAC_CTRL_CONVMODE_CONTINUOUS, dacConvModeSampleHold = _DAC_CTRL_CONVMODE_SAMPLEHOLD, dacConvModeSampleOff = _DAC_CTRL_CONVMODE_SAMPLEOFF } | 
| Conversion mode. | |
| enum | DAC_Output_TypeDef
         
         { dacOutputDisable = _DAC_CTRL_OUTMODE_DISABLE, dacOutputPin = _DAC_CTRL_OUTMODE_PIN, dacOutputADC = _DAC_CTRL_OUTMODE_ADC, dacOutputPinADC = _DAC_CTRL_OUTMODE_PINADC } | 
| Output mode. | |
| enum | DAC_PRSSEL_TypeDef
         
         { dacPRSSELCh0 = _DAC_CH0CTRL_PRSSEL_PRSCH0, dacPRSSELCh1 = _DAC_CH0CTRL_PRSSEL_PRSCH1, dacPRSSELCh2 = _DAC_CH0CTRL_PRSSEL_PRSCH2, dacPRSSELCh3 = _DAC_CH0CTRL_PRSSEL_PRSCH3, dacPRSSELCh4 = _DAC_CH0CTRL_PRSSEL_PRSCH4, dacPRSSELCh5 = _DAC_CH0CTRL_PRSSEL_PRSCH5, dacPRSSELCh6 = _DAC_CH0CTRL_PRSSEL_PRSCH6, dacPRSSELCh7 = _DAC_CH0CTRL_PRSSEL_PRSCH7, dacPRSSELCh8 = _DAC_CH0CTRL_PRSSEL_PRSCH8, dacPRSSELCh9 = _DAC_CH0CTRL_PRSSEL_PRSCH9, dacPRSSELCh10 = _DAC_CH0CTRL_PRSSEL_PRSCH10, dacPRSSELCh11 = _DAC_CH0CTRL_PRSSEL_PRSCH11 } | 
| Peripheral Reflex System signal used to trigger single sample. | |
| enum | DAC_Ref_TypeDef
         
         { dacRef1V25 = _DAC_CTRL_REFSEL_1V25, dacRef2V5 = _DAC_CTRL_REFSEL_2V5, dacRefVDD = _DAC_CTRL_REFSEL_VDD } | 
| Reference voltage for DAC. | |
| enum | DAC_Refresh_TypeDef
         
         { dacRefresh8 = _DAC_CTRL_REFRSEL_8CYCLES, dacRefresh16 = _DAC_CTRL_REFRSEL_16CYCLES, dacRefresh32 = _DAC_CTRL_REFRSEL_32CYCLES, dacRefresh64 = _DAC_CTRL_REFRSEL_64CYCLES } | 
| Refresh interval. | |
Function Documentation
◆ DAC_Enable()
| void DAC_Enable | ( | DAC_TypeDef * | 
            dac,
            | 
| unsigned int | 
            ch,
            | ||
| bool | 
            enable
            | ||
| ) | 
Enable/disable the DAC channel.
- Parameters
- 
         [in] dacA pointer to the DAC peripheral register block. [in] chA channel to enable/disable. [in] enabletrue to enable DAC channel, false to disable. 
◆ DAC_Init()
| void DAC_Init | ( | DAC_TypeDef * | 
            dac,
            | 
| const DAC_Init_TypeDef * | 
            init
            | ||
| ) | 
Initialize DAC.
Initializes common parts for both channels. In addition, channel control configuration must be done. See DAC_InitChannel() .
- Note
- This function will disable both channels prior to configuration.
- Parameters
- 
         [in] dacA pointer to the DAC peripheral register block. [in] initA pointer to the DAC initialization structure. 
◆ DAC_InitChannel()
| void DAC_InitChannel | ( | DAC_TypeDef * | 
            dac,
            | 
| const DAC_InitChannel_TypeDef * | 
            init,
            | ||
| unsigned int | 
            ch
            | ||
| ) | 
Initialize DAC channel.
- Parameters
- 
         [in] dacA pointer to the DAC peripheral register block. [in] initA pointer to the DAC initialization structure. [in] chA channel number to initialize. 
◆ DAC_ChannelOutputSet()
| void DAC_ChannelOutputSet | ( | DAC_TypeDef * | 
            dac,
            | 
| unsigned int | 
            channel,
            | ||
| uint32_t | 
            value
            | ||
| ) | 
Set the output signal of a DAC channel to a given value.
        This function sets the output signal of a DAC channel by writing
        
         value
        
        to the corresponding CHnDATA register.
       
- Parameters
- 
         [in] dacA pointer to the DAC peripheral register block. [in] channelA channel number to set the output. [in] valueA value to write to the channel output register CHnDATA. 
◆ DAC_Channel0OutputSet()
| 
 | inline | 
Set the output signal of DAC channel 0 to a given value.
        This function sets the output signal of DAC channel 0 by writing
        
         value
        
        to the CH0DATA register.
       
- Parameters
- 
         [in] dacPointer to DAC peripheral register block. [in] valueValue to write to the channel 0 output register CH0DATA. 
◆ DAC_Channel1OutputSet()
| 
 | inline | 
Set the output signal of DAC channel 1 to a given value.
        Sets the output signal of DAC channel 1 by writing
        
         value
        
        to the CH1DATA register.
       
- Parameters
- 
         [in] dacPointer to DAC peripheral register block. [in] valueValue to write to the channel 1 output register CH1DATA. 
◆ DAC_IntClear()
| 
 | inline | 
Clear one or more pending DAC interrupts.
- Parameters
- 
         [in] dacPointer to DAC peripheral register block. [in] flagsPending DAC interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the DAC module (DAC_IF_nnn). 
◆ DAC_IntDisable()
| 
 | inline | 
Disable one or more DAC interrupts.
- Parameters
- 
         [in] dacPointer to DAC peripheral register block. [in] flagsDAC interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the DAC module (DAC_IF_nnn). 
◆ DAC_IntEnable()
| 
 | inline | 
Enable one or more DAC interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using DAC_IntClear() prior to enabling the interrupt.
- Parameters
- 
         [in] dacPointer to DAC peripheral register block. [in] flagsDAC interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the DAC module (DAC_IF_nnn). 
◆ DAC_IntGet()
| 
 | inline | 
Get pending DAC interrupt flags.
- Note
- Event bits are not cleared by the use of this function.
- Parameters
- 
         [in] dacPointer to DAC peripheral register block. 
- Returns
- DAC interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for the DAC module (DAC_IF_nnn).
◆ DAC_IntGetEnabled()
| 
 | inline | 
Get enabled and pending DAC interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Parameters
- 
         [in] dacPointer to DAC peripheral register block. 
- Note
- Interrupt flags are not cleared by the use of this function.
- Returns
- 
         Pending and enabled DAC interrupt sources. Return value is the bitwise AND combination of
         - the OR combination of enabled interrupt sources in DACx_IEN_nnn register (DACx_IEN_nnn) and
- the OR combination of valid interrupt flags of the DAC module (DACx_IF_nnn).
 
◆ DAC_IntSet()
| 
 | inline | 
Set one or more pending DAC interrupts from SW.
- Parameters
- 
         [in] dacPointer to DAC peripheral register block. [in] flagsDAC interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the DAC module (DAC_IF_nnn). 
◆ DAC_PrescaleCalc()
| uint8_t DAC_PrescaleCalc | ( | uint32_t | 
            dacFreq,
            | 
| uint32_t | 
            hfperFreq
            | ||
| ) | 
Calculate prescaler value used to determine the DAC clock.
The DAC clock is given by: HFPERCLK / (prescale ^ 2). If the requested DAC frequency is low and the maximum prescaler value can't adjust the actual DAC frequency lower than the requested DAC frequency, the maximum prescaler value is returned resulting in a higher DAC frequency than requested.
- Parameters
- 
         [in] dacFreqDAC frequency wanted. The frequency will automatically be adjusted to be below the maximum allowed DAC clock. [in] hfperFreqFrequency in Hz of the reference HFPER clock. Set to 0 to use the currently defined HFPER clock setting. 
- Returns
- 
         Prescaler value to use for DAC to achieve a clock value <=
         dacFreq.
◆ DAC_Reset()
| void DAC_Reset | ( | DAC_TypeDef * | 
            dac
            | ) | 
Reset DAC to the same state that it was in after a hardware reset.
- Parameters
- 
         [in] dacA pointer to the ADC peripheral register block. 
Macro Definition Documentation
◆ DAC_INIT_DEFAULT
| #define DAC_INIT_DEFAULT | 
Default configuration for DAC initialization structure.
◆ DAC_INITCHANNEL_DEFAULT
| #define DAC_INITCHANNEL_DEFAULT | 
Default configuration for DAC channel initialization structure.
Enumeration Type Documentation
◆ DAC_ConvMode_TypeDef
| enum DAC_ConvMode_TypeDef | 
◆ DAC_Output_TypeDef
| enum DAC_Output_TypeDef | 
◆ DAC_PRSSEL_TypeDef
| enum DAC_PRSSEL_TypeDef | 
Peripheral Reflex System signal used to trigger single sample.
◆ DAC_Ref_TypeDef
| enum DAC_Ref_TypeDef | 
◆ DAC_Refresh_TypeDef
| enum DAC_Refresh_TypeDef |