LESENSE_DecCtrlDesc_TypeDef Struct Reference
LESENSE decoder control descriptor structure.
      
       #include <em_lesense.h>
      
     
| Data Fields | |
| LESENSE_DecInput_TypeDef | decInput | 
| Select input to the LESENSE decoder. | |
| uint32_t | initState | 
| Initial state of the LESENSE decoder. | |
| bool | chkState | 
| Set to enable decoder to check the present state in addition to the states defined in TCONF. | |
| bool | intMap | 
| When set, a transition from state x in decoder will set the interrupt flag CHx. | |
| bool | hystPRS0 | 
| Set to enable hysteresis in decoder for suppressing the changes on PRS channel 0. | |
| bool | hystPRS1 | 
| Set to enable hysteresis in decoder for suppressing the changes on PRS channel 1. | |
| bool | hystPRS2 | 
| Set to enable hysteresis in decoder for suppressing the changes on PRS channel 2. | |
| bool | hystIRQ | 
| Set to enable hysteresis in decoder for suppressing the interrupt requests. | |
| bool | prsCount | 
| Set to enable count mode on decoder PRS channels 0 and 1 to produce outputs which can be used by a PCNT to count up or down. | |
| LESENSE_PRSSel_TypeDef | prsChSel0 | 
| Select PRS channel input for bit 0 of LESENSE decoder. | |
| LESENSE_PRSSel_TypeDef | prsChSel1 | 
| Select PRS channel input for bit 1 of LESENSE decoder. | |
| LESENSE_PRSSel_TypeDef | prsChSel2 | 
| Select PRS channel input for bit 2 of LESENSE decoder. | |
| LESENSE_PRSSel_TypeDef | prsChSel3 | 
| Select PRS channel input for bit 3 of LESENSE decoder. | |
LESENSE decoder control descriptor structure.
Field Documentation
◆ decInput
| LESENSE_DecInput_TypeDef LESENSE_DecCtrlDesc_TypeDef::decInput | 
Select input to the LESENSE decoder.
◆ initState
| uint32_t LESENSE_DecCtrlDesc_TypeDef::initState | 
Initial state of the LESENSE decoder.
◆ chkState
| bool LESENSE_DecCtrlDesc_TypeDef::chkState | 
Set to enable decoder to check the present state in addition to the states defined in TCONF.
◆ intMap
| bool LESENSE_DecCtrlDesc_TypeDef::intMap | 
When set, a transition from state x in decoder will set the interrupt flag CHx.
◆ hystPRS0
| bool LESENSE_DecCtrlDesc_TypeDef::hystPRS0 | 
Set to enable hysteresis in decoder for suppressing the changes on PRS channel 0.
◆ hystPRS1
| bool LESENSE_DecCtrlDesc_TypeDef::hystPRS1 | 
Set to enable hysteresis in decoder for suppressing the changes on PRS channel 1.
◆ hystPRS2
| bool LESENSE_DecCtrlDesc_TypeDef::hystPRS2 | 
Set to enable hysteresis in decoder for suppressing the changes on PRS channel 2.
◆ hystIRQ
| bool LESENSE_DecCtrlDesc_TypeDef::hystIRQ | 
Set to enable hysteresis in decoder for suppressing the interrupt requests.
◆ prsCount
| bool LESENSE_DecCtrlDesc_TypeDef::prsCount | 
Set to enable count mode on decoder PRS channels 0 and 1 to produce outputs which can be used by a PCNT to count up or down.
◆ prsChSel0
| LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel0 | 
Select PRS channel input for bit 0 of LESENSE decoder.
◆ prsChSel1
| LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel1 | 
Select PRS channel input for bit 1 of LESENSE decoder.
◆ prsChSel2
| LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel2 | 
Select PRS channel input for bit 2 of LESENSE decoder.
◆ prsChSel3
| LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel3 | 
Select PRS channel input for bit 3 of LESENSE decoder.