WDOG_Init_TypeDef Struct Reference
Watchdog initialization structure.
      
       #include <em_wdog.h>
      
     
| Data Fields | |
| bool | enable | 
| Enable Watchdog when initialization completed. | |
| bool | debugRun | 
| Counter keeps running during debug halt. | |
| bool | clrSrc | 
| Select WDOG clear source: False: Write to the clear bit will clear the WDOG counter True: Rising edge on the PRS Source 0 will clear the WDOG counter. | |
| bool | em1Run | 
| Counter keeps running when in EM1. | |
| bool | em2Run | 
| Counter keeps running when in EM2. | |
| bool | em3Run | 
| Counter keeps running when in EM3. | |
| bool | em4Block | 
| Block EMU from entering EM4. | |
| bool | prs0MissRstEn | 
| When set, a PRS Source 0 missing event will trigger a WDOG reset. | |
| bool | prs1MissRstEn | 
| When set, a PRS Source 1 missing event will trigger a WDOG reset. | |
| bool | lock | 
| Block SW from disabling LFRCO/LFXO oscillators. | |
| WDOG_PeriodSel_TypeDef | perSel | 
| Clock source to use for Watchdog. | |
| WDOG_WarnSel_TypeDef | warnSel | 
| Select warning time as % of the Watchdog timeout. | |
| WDOG_WinSel_TypeDef | winSel | 
| Select illegal window time as % of the Watchdog timeout. | |
| bool | resetDisable | 
| Disable Watchdog reset output if true. | |
Watchdog initialization structure.
Field Documentation
◆ enable
| bool WDOG_Init_TypeDef::enable | 
Enable Watchdog when initialization completed.
◆ debugRun
| bool WDOG_Init_TypeDef::debugRun | 
Counter keeps running during debug halt.
◆ clrSrc
| bool WDOG_Init_TypeDef::clrSrc | 
Select WDOG clear source: False: Write to the clear bit will clear the WDOG counter True: Rising edge on the PRS Source 0 will clear the WDOG counter.
◆ em1Run
| bool WDOG_Init_TypeDef::em1Run | 
Counter keeps running when in EM1.
Available for series2.
◆ em2Run
| bool WDOG_Init_TypeDef::em2Run | 
Counter keeps running when in EM2.
◆ em3Run
| bool WDOG_Init_TypeDef::em3Run | 
Counter keeps running when in EM3.
◆ em4Block
| bool WDOG_Init_TypeDef::em4Block | 
Block EMU from entering EM4.
◆ prs0MissRstEn
| bool WDOG_Init_TypeDef::prs0MissRstEn | 
When set, a PRS Source 0 missing event will trigger a WDOG reset.
◆ prs1MissRstEn
| bool WDOG_Init_TypeDef::prs1MissRstEn | 
When set, a PRS Source 1 missing event will trigger a WDOG reset.
◆ lock
| bool WDOG_Init_TypeDef::lock | 
Block SW from disabling LFRCO/LFXO oscillators.
Block SW from modifying the configuration (a reset is needed to reconfigure).
◆ perSel
| WDOG_PeriodSel_TypeDef WDOG_Init_TypeDef::perSel | 
Clock source to use for Watchdog.
Watchdog timeout period.
◆ warnSel
| WDOG_WarnSel_TypeDef WDOG_Init_TypeDef::warnSel | 
Select warning time as % of the Watchdog timeout.
◆ winSel
| WDOG_WinSel_TypeDef WDOG_Init_TypeDef::winSel | 
Select illegal window time as % of the Watchdog timeout.
◆ resetDisable
| bool WDOG_Init_TypeDef::resetDisable | 
Disable Watchdog reset output if true.