LETIMER_Init_TypeDef Struct Reference
LETIMER initialization structure.
#include <em_letimer.h>
Data Fields | |
bool | enable |
Start counting when initialization completes. | |
bool | debugRun |
Counter shall keep running during debug halt. | |
bool | rtcComp0Enable |
Start counting on RTC COMP0 match. | |
bool | rtcComp1Enable |
Start counting on RTC COMP1 match. | |
bool | comp0Top |
Load COMP0 register into CNT when counter underflows. | |
bool | bufTop |
Load COMP1 into COMP0 when REP0 reaches 0. | |
uint8_t | out0Pol |
Idle value for output 0. | |
uint8_t | out1Pol |
Idle value for output 1. | |
LETIMER_UFOA_TypeDef | ufoa0 |
Underflow output 0 action. | |
LETIMER_UFOA_TypeDef | ufoa1 |
Underflow output 1 action. | |
LETIMER_RepeatMode_TypeDef | repMode |
Repeat mode. | |
uint32_t | topValue |
Top value. | |
LETIMER initialization structure.
Field Documentation
◆ enable
bool LETIMER_Init_TypeDef::enable |
Start counting when initialization completes.
◆ debugRun
bool LETIMER_Init_TypeDef::debugRun |
Counter shall keep running during debug halt.
◆ rtcComp0Enable
bool LETIMER_Init_TypeDef::rtcComp0Enable |
Start counting on RTC COMP0 match.
◆ rtcComp1Enable
bool LETIMER_Init_TypeDef::rtcComp1Enable |
Start counting on RTC COMP1 match.
◆ comp0Top
bool LETIMER_Init_TypeDef::comp0Top |
Load COMP0 register into CNT when counter underflows.
◆ bufTop
bool LETIMER_Init_TypeDef::bufTop |
Load COMP1 into COMP0 when REP0 reaches 0.
◆ out0Pol
uint8_t LETIMER_Init_TypeDef::out0Pol |
Idle value for output 0.
◆ out1Pol
uint8_t LETIMER_Init_TypeDef::out1Pol |
Idle value for output 1.
◆ ufoa0
LETIMER_UFOA_TypeDef LETIMER_Init_TypeDef::ufoa0 |
Underflow output 0 action.
◆ ufoa1
LETIMER_UFOA_TypeDef LETIMER_Init_TypeDef::ufoa1 |
Underflow output 1 action.
◆ repMode
LETIMER_RepeatMode_TypeDef LETIMER_Init_TypeDef::repMode |
Repeat mode.
◆ topValue
uint32_t LETIMER_Init_TypeDef::topValue |
Top value.
Counter wraps when top value matches counter value is reached.